It’s funny - we are getting braver and braver with our soldering skills. Hence, we are getting smaller and smaller packages. QFNs are now standard issue around the office. Our eyes hate us for it :shock:
I was shaking like crazy the first time I soldered a ‘surface mount’ part. The ADXL 202 was so small. But with a little practice, you’re confidence comes up and soldering smaller and smaller devices becomes cake.
These are my recommendations in order of importance:
Get a good soldering iron. $10 is too much to spend! What I mean is this - you can’t do squat with a $10 iron if you need to do SMD. Throw the thing away and spend $90 and get a Weller WES51. I’ve got a WES50 that we’ve been using for years without a hickup. You can always drop the big one and get a $500 Metcal but I did not experience that much of a difference.
Get good solder wick. I use ‘TechSpray 1815-5F’? No clean wick, .055" width. But the part number is not that important. Get a good grade wick. $0.90 is useless. $20 is ridiculous. This was $2.51 for 5’ or something. Works like a charm!
Hemostats are good. Tweezer work well.
Lighting is important - you’ve got to see!
Magnifying glass is nice, but I never use it. Nothing against ken (old man
) but if you’re eyes are good, or if your prescription is up to date, you can see even the smallest jumper problems without the Ghost Busters’ eye magnifiers.
Here’s how I do a tiny, tiny, QFN package. We don’t do any board prep. Get your board and your iron, clean your tip, and throw a blob of solder on pads 1 and 2. Jumper them with a good blob. Next clean your tip. Next, take your QFN (or other) part with the tweezers. Next, clean your tip. Then heat the blob with the iron and slide the QFN part horizontally into the blob. You can do vertically, but it will tend to push the solder the wrong way. Once you have close alignment, hold the part still and take the iron away - pause, release the part. Does it look lined up? No? Hold the part, heat the blob, tweak the alignment ever so slightly. This is where practice comes into play. We can usually line up a part on the first or second try.
Once you’ve got good alignment, take a big blob of solder on your tip and run it down the opposite side of the chip. A little flux helps, and little practice is worth even more. Leadless chips are great because they tend to hold the surface tension of the solder better than SOIC or SSOP leaded chips. Repeat for all sides.
A quick inspection will show leads that you need to touch up.
I taught a history major how to solder in a few days. Through hole, to SSOP, to QFN. He’s now lightning fast and better than I. :roll:
With all that said, I am currently drooling over a $20k pick a place machine with reflow oven… Hmmm…
http://www.madelltech.com/m2-2.html
-Nathan