I would like to built a 18F97J60 board, but this Pic is TQFT 100 package and not easy to solder on a home made board without special SMT tools. ( too thin pins )
Is there some adaptors available on the market for this package, or maybe a way build home made board with that Pic ?
TQFP can be soldered by hand, spark fun has a great SMD soldering tutorial in their tutorials section.
We solder 208 pin PQFP with fine pitch by using a hot air rework machine where I work, we’ve soldered 144 pin TQFP’s by hand with a fine tip solder iron on occasion.
You don’t even need a fine-tipped soldering iron, any iron will do. You just need solder and desoldering braid. Flux helps. A good magnifying glass or microscope is almost essential.
Apply flux. Position the chip correctly (the hard part). Using two pairs of tweezers and some kind of hands-free magnifying device is the best way. Optionally tack one corner pin down with solder. Cover one whole row of pins with lots o’ solder. Repeat for the other 4 rows, then use braid to remove it, leaving a nicely soldered chip! Inspect with the magnifying glass for shorts and open pins (poke each pin with tweezers, if it moves it’s not soldered).
On the other hand, removing a TQFP without hot air or IR is very difficult.
there are a number of web sites that can take you through making PCBs at home. There are two ways people use:
photo exposure
toner transfer
photo will get you finer lines and I know people have done QFNs that way. Toner transfer is a bit harder to get to work for fine pitch but it is possible.
Also, thought I’d jump in here to note something I’ve had lots of success with. If you’d rather spend the $5 on a complete breakout board with soldermask and a ground plane, instead of copper clad, toner transfers, and etching chemicals, I’ve had a lot of luck with Schmartboards:
They have boards for many parts in many pitches, and have even started making BGA breakouts recently. I have used their normal, cheaper boards (not the EZ ones) with a little bit of solder paste, and it works like a dream.
leon_heller:
Drag-soldering works very well. I use a Metcal system with a mini-hoof cartridge, but you can use an ordinary tip.
Leon
Yup - no need for hot air. I wouldn’t use a $5 soldering pencil but any decent quality soldering iron will work fine. You don’t need an expensive tool. There’s a video floating around the internet of someone using a huge soldering iron doing some sort of TQFP. The tip must be an inch (er, 25.4 mm) across.
You will also want to use liquid flux - it really helps.