htc desire to picaxe 28x2 via bluesmirf

Hi, I’m trying to use a htc desire phone to connect to a picaxe 28x2 via a bluesmirf reciever but it doesn’t seem to work.

septr increments by 1 with each send even when 10 bytes are sent.

The picaxe only seems to get one byte of rubbish, mainly 255.

I’ve tried various baud rates but no luck.

any ideas ?

thanks

Code below:

’ bluesmirf set at 9600

hsersetup B9600_8, %011 ’ septr increments by 1 with each send but picaxe receives rubbish

main:

debug

pause 500

if hserptr <> 0 then

pause 1000

gosub getScratchPad

’ hserptr = 0

’ hserinflag = 0

endif

goto main

end

'-------------------------------------------------------------

getScratchPad:

get 0, b0

get 1, b1

get 2, b2

get 3, b3

get 4, b4

get 5, b5

return