Hi,
I have a ConnectPort X2 that I want to run some python code on. From the Digi documentation it seems that I need the web interface running to upload my python files to the device. However, I cannot access the device using a web browser.
I can telnet and check the service status. Sure enough, the HTTP service is not running on the device. Here is the output for set service command:
#> set service
Service Configuration :
index state ipport keepalive nodelay dlyd-ack service
1 off 7 off off 200 TCP Echo Service
2 off 7 na na 200 UDP Echo Service
3 on 23 on off 200 Telnet Service
4 on 2362 na na 200 ADDP Service
I have tried rebooting the device and “revert service” to default the device to start HTTP, but they have not worked. Here is some information from display device that might be useful.
Product : ConnectPort X2
Firmware Version : 2.13.0.10 (Version 82002458_B 05/02/2011)
Boot Version : 1.1.2 (release_82001228_A)
Post Version : 1.1.3 (release_82002307_D)
Thanks a lot for the help. I am new to Connectports, so please excuse me if I missed something glaringly obvious.
regards,
A