I have a load cell that has a max excitation voltage of 12V. Using the HX711 it will only be powered at 5V (I think?), thus decreasing the sensitivity of the load cell output (mV/V).
Can I power the load cell with 12V (obviously grounding the HX711 and load cell together) or will I destroy the HX711?
I think you’re asking if you can use external excitation. Yes, that will get you more signal from the transducer for a given load. Of course, you’ll have to ensure that the ADC input isn’t exceeded and that the power supply is very quiet and stable.