Even if you know it’s there, it’s not easy to find. Sparkfun search is really pretty bad. They have so many products now that the search is getting more important.
So, looking at those two boards, they don’t seem to be TRUE Level shifters. They only bring down +/- 12V logic to 5V, but do not go the other way. (No charge pumps to increase 5V to +/- 12V).
This may be ok for connecting a uController to a tolerant PC, but I am trying to connect a uController to a true RS-232 device (an X-10 serial controller). Neither of those boards will work. And shame on sparkfun for not being clear on this. One board does admit it’s only EIA-232, but the other one does not.
So I repeat my initial request for a TRUE MAX232 logic level shifter breakout.
I too just spent a little while searching for this… problem I guess is most of the time people are doing USB=>Serial now so go direct from USB to 5V.
I too have a device I want to interface with that is RS232… and you are right there are no dedicated proper RS232 convertors… only “EIA-232” ones that do basically +/- 5V.
I know it’s slightly naughty to advertise a competitor on a competitors board, but since sparkfun don’t actually sell this product I guess it should be OK.
n1ist, I don’t want something big and bulky like a pic development board, that last one looks like it is true RS-232, but it was built to sit in a Xbee slot which i have no use for.