I am going to have a project which needs to convert signal (4800bps) between 5v and 12V. I see that there is a breakout board for 3.3v <—> 5v but not for 5v<—>12v. Does Sparkfun have a breakout board for signal conversion between 5V and 12V?
No. As described in my post and the title, what I need is 5v<–>12v (or more precisely, 0/5v <—> 0/12v), not TTL to/from RS-232 (which is 0/5v<–> -12/+12v).
EddyL:
No. As described in my post and the title, what I need is 5v<–>12v (or more precisely, 0/5v <—> 0/12v), not TTL to/from RS-232 (which is 0/5v<–> -12/+12v).
Or to be exact, MAX3232 inverts and shifts logic level between 0v/5v <—> -6v/+6v (or -12v/+12v) as what my MAX3232 showed me in my another project. This is not what I need here.
If there is no readily made Sparkfund board which can do the 0v-5v<—>0v-12v conversion, I will appreciate it if anyone can give me some suggestion how I can get the same result. I understand that a simple transistor/resistor circuit should be able to do this conversion but I do not have the ability to design one.
Checkout Philips AN97055; that configuration should work for any voltages as long as the mosfets can tolerate the higher voltages and can operate at the lowest ones.
Thanks a lot for the repy and information. I have just placed an order for the “SparkFun Logic Level Converter - Bi-Directional” and will give it a try for 5v<—>12v conversion.
languer:
Checkout Philips AN97055; that configuration should work for any voltages as long as the mosfets can tolerate the higher voltages and can operate at the lowest ones.
A little late here; but I’m glad it worked. And thanks for coming back and letting the community know it worked; perhaps it will also help someone with a similar need in the future.