I got that ET-JRAVR board but the schematic is wrong:
http://s193925491.onlinehome.us/Futurle … ematic.jpg
Does anyone have an updated schematic or the Protel file which can be edited and correcitons made.
The manual is also wrong:
http://s193925491.onlinehome.us/Futurle … tBoard.pdf
This board comes from a Thai maker:
http://www.etteam.com/product/03000AVR.html
http://www.etteam.com/product/pics/03AV … /JRAVR.jpg
I got it from Futurlec and I can confirm that pins do not reflect the PDF schematic.
Thanks
B
email ETT. I have found them to be very supportive for their products I’ve ordered.
stevech:
email ETT. I have found them to be very supportive for their products I’ve ordered.
Yes, you are correct.
Very true, they were helpful. Thank you.
After digging I found great new manual and new CORRECT schematic of the JRAVR board. Here is the info:
[CP-jrAVR_Schematic.pdf
[CP-JRAVRUsersManual.pdf
Hope that will be useful to all!
~B](http://s193925491.onlinehome.us/futurlecboard/CP-JRAVRUsersManual.pdf)](http://s193925491.onlinehome.us/futurlecboard/CP-jrAVR_Schematic.pdf)
Now that I got the schematic figured out my first code to run a little $5 LED board I got on eBay that uses SPI-line interface:
http://s193925491.onlinehome.us/Futurle … P001-5.jpg
#include <avr/io.h>
#include <util/delay.h>
const unsigned char Digital_TAB[] = {0xff,0xfc,0x60,0xda,0xf2,0x66,0xb6,0xbe,0xe0,0xfe,0xf6, 0x80,0x40,0x20,0x10,0x08,0x04,0x02,0x01};
int U, j, i;
void main(void) //main function starts here
{
DDRB=0xFF;
while (1==1){ //cycle forever - main loop
for(j = 0; j <19; j++) //symbol from array 1-2-3-A-B-C-etc
{
U = Digital_TAB[j];
PORTB |= (1<<PINB3); //turn OFF display, LOW pin 3
for(i = 0;i < 8; i++) //character shift out ISP routine
{
PORTB = (PORTB & ~(1<<PINB1)) | ((U & 0x01)<<PINB1);
PORTB |= (1<<PINB2);
PORTB &= ~(1<<PINB2);
U = U>>1;
}
PORTB &= ~(1<<PINB3); //turn ON display, HIGH pin 3
_delay_ms(100);
}
}
}
Woo hoo, it works. That Atmel board is actually very useful for these kinds of tests.
But bottom line is - you are correct, ETT did help
Thanks
~B
http://s193925491.onlinehome.us/Futurle … 08_002.jpg
http://s193925491.onlinehome.us/Futurle … 08_001.jpg