IAR Kickstart with Olimex's MSP430F2131 header board

Hi,

How do I load code onto the 2131 chip that’s on a JTAG header board using IAR Kickstart?

I have the latest version of the software and the latest drivers. I’m trying to load a program onto Olimex’s MSP430F2131 header board via a TI USB-FET. Does the Debug command compile and load the code onto the uC? In IAR’s options, the device is set to MSP430F2131, debugger driver is set to FET Debugger and FET-Debugger is set to TI USB-IF.

I’ve been trying to load a sample LED flashing program onto the uC on this board and I just can’t do it. Please help me…