Import MDM, Module not responding

I am new to both python and GM862 module. I have a GM862 with the usb evaluation board.

Type : GM862-GPS

IMEI : 358278000239681

IC : 5131A-GM862G

LOT N : 4606 7S024013H00

Currently using

python version: 2.5.4

python win:pywin32-210.win32-py2.5

python serial: pyserial-2.4.win32

Set the “com5” in the MDM.py (COM5, this is the port I set the hyper terminal to get the module to work). The module is working through hyper terminal. When I open the python IDLE and type in “import MDM” , I a popup with the warning “module not responding do you want to retry”. YES repeats the popup, NO gives the following message in the IDLE

Traceback (most recent call last):

File “<pyshell#0>”, line 1, in

import MDM

File “C:\Python25\lib\site-packages\Pythonwin\MDM.py”, line 104, in

raise StandardError, ‘ERROR: The module is not responding!’

StandardError: ERROR: The module is not responding![/code]

Any ideas of how to get the python import MDM module to work…

Regards,

Badri

email:bkbn@engineer.com

Ph:9373672398