Hi Sparkfun Community,
I am using the Analog MEMS Microphone Breakout Board (SPH8878LR5H-1)  for audio input into a line level recorder. Unless the sound is coming very close to the mic it is too quiet.
Does anyone know if there is a way to increase the gain on the Op Amp Circuit? Looks like I would have to swap out an SMD component to do so, any advice or pointers? I like the quality of the audio but just need to be able to pickup quieter sounds too.
Thanks in advance for any guidance!
             
            
              1 Like 
            
            
           
          
            
            
              To increase the gain, increase the ratio R4/R3. R4 = 300K for x64, R4 = 1Meg for x213.
You may run into oscillation or stability problems if you increase the gain too much, as the gain-bandwidth product of the OPA344 is only 1 MHz.
             
            
              3 Likes 
            
            
           
          
            
            
              Awesome, thank you! So I should be able to just replace R4 with say a 500K (ie. 504 code SMD) and it should increase the gain a bit?
             
            
              
            
           
          
            
            
              In that case, use a gain of 1, not 0. Replace the feedback resistor with 4.7K.
Hint:   gain = (output voltage)/(input voltage)
             
            
              1 Like 
            
            
           
          
            
            
              Digi-Key has 3.2 million of them in stock, 100 of them are less than a dollar.
  
  
    Order today, ships today. RC0603JR-074K7L – 4.7 kOhms ±5% 0.1W, 1/10W Chip Resistor 0603 (1608 Metric) Moisture Resistant Thick Film from YAGEO. Pricing and Availability on millions of electronic components from Digi-Key Electronics.
   
  
    
    
  
  
 
             
            
              1 Like