I’ve seen some temperature controlled solder iron + hot-air stations on ebay for roughly $100-125 (USD). I was wondering if those are just crap that’s going to annoy me and burn out. Keep in mind that I’ve been using the same $15 soldering iron I got 30 years ago as a kid :roll: … with the same tip. :shock:
I’m not above working with/around some shortcomings, but I want good value, and I’m on the verge of diving into SMD board designs. Since electronics is just a rainy day hobby, it won’t get a ton of use.
Thats the standard set of Aoyue stations. The hot air works, and for the price, is a great value. However, the soldering iron is passable at best.
I would seriously consider a standalone soldering station, and if you need hot air get a standalone hot air station. Hakko will give you a great value for soldering stations (plus their tips are long lived). As its light use, suggesting a Metcal is out of the question
I concur with theatrus; I’ve got a very similar Chinese rework station, and it’s great value just for the hot air function.
The soldering iron isn’t great, but I found a lot of the problem is the tips. Replacing the supplied tip with a genuine Hakko tip (they are compatible, at least the ones I saw) made a HUGE difference. There was too much “slop” in the fit of the original tip fitting over the ceramic heating element, which resulted in very poor transfer of heat.
Anyway, I don’t use the soldering iron on my station, since I have a real Hakko soldering iron, which is great…
I have the Auyue 968 and I find the soldering iron to be perfectly workable. I need to get a new tip, though. The pointy/needle like tip that came with it, works, but I’d like a small wedge one.
Curious…given that many deals include a choice of tips (up to 10 in some cases), what tips do you suggest? I’m guessing there are only 2-3 common choices and I’ll get a few of each.
and never had any problem. The three were bought separately with a few months between each puchase. Good inexpensive stuff.
They are also compatible with Kada iron tips (900M-T).
I like the 900M-T-B for general SMD work, and the 900M-T-K chisel to solder fine pitch IC like TQFP. You add solder and then you wipe it on the pins while moving away from the chip to get a really clean finish.