I have a GPS RTK2 - Zed F9P board hooked to a raspberry pi with the following connections.
Rpi TX → Rtk RX2
Rpi RX → Rtk TX2
Ground - Ground
5v - 5v
On the raspberry pi I am running the following code to connect to an NTRIP base station and then try to send the RTCM3 data into the GPS RTK2 board through the rpi serial port. However, when I run the code, and I check U-Center, the GPS is not going into RTK mode. Do I have the Serial.Write in the correct place? Not sure what is going on here. I am running ntrip.py (ntrip.py needs rtcm3.py as an import)
ntrip.py
"""
 NTRIP client module
 based on client from http://github.com/jcmb/NTRIP
"""
import socket
import sys
import datetime
import base64
import time
import errno
import rtcm3
import ssl
from optparse import OptionParser
import serial
version = 0.1
useragent = "NTRIP MAVProxy/%.1f" % version
class NtripError(Exception):
    def __init__(self, message, inner_exception=None):
        self.message = message
        self.inner_exception = inner_exception
        self.exception_info = sys.exc_info()
    def __str__(self):
        return self.message
class NtripClient(object):
    def __init__(self,
                 user="",
                 port=2101,
                 caster="",
                 mountpoint="",
                 host=False,
                 lat=46,
                 lon=122,
                 height=1212,
                 ssl=False,
                 V2=False,
                 ):
        if sys.version_info.major >= 3:
            user = bytearray(user, 'ascii')
        self.user = base64.b64encode(user)
        self.port = port
        self.caster = caster
        self.mountpoint = mountpoint
        if not self.mountpoint.startswith("/"):
            self.mountpoint = "/" + self.mountpoint
        self.setPosition(lat, lon)
        self.height = height
        self.ssl = ssl
        self.host = host
        self.V2 = V2
        self.socket = None
        self.found_header = False
        self.sent_header = False
        # RTCM3 parser
        self.rtcm3 = rtcm3.RTCM3()
        self.last_id = None
        if self.port == 443:
            # force SSL on port 443
            self.ssl = True
    def setPosition(self, lat, lon):
        self.flagN = "N"
        self.flagE = "E"
        if lon > 180:
            lon = (lon-360)*-1
            self.flagE = "W"
        elif lon < 0 and lon >= -180:
            lon = lon*-1
            self.flagE = "W"
        elif lon < -180:
            lon = lon+360
            self.flagE = "E"
        else:
            self.lon = lon
        if lat < 0:
            lat = lat*-1
            self.flagN = "S"
        self.lonDeg = int(lon)
        self.latDeg = int(lat)
        self.lonMin = (lon-self.lonDeg)*60
        self.latMin = (lat-self.latDeg)*60
    def getMountPointString(self):
        userstr = self.user
        if sys.version_info.major >= 3:
            userstr = str(userstr, 'ascii')
        mountPointString = "GET %s HTTP/1.0\r\nUser-Agent: %s\r\nAuthorization: Basic %s\r\n" % (
            self.mountpoint, useragent, userstr)
        if self.host or self.V2:
            hostString = "Host: %s:%i\r\n" % (self.caster, self.port)
            mountPointString += hostString
        if self.V2:
            mountPointString += "Ntrip-Version: Ntrip/2.0\r\n"
        mountPointString += "\r\n"
        return mountPointString
    def getGGAString(self):
        now = datetime.datetime.utcnow()
        ggaString = "GPGGA,%02d%02d%04.2f,%02d%011.8f,%1s,%03d%011.8f,%1s,1,05,0.19,+00400,M,%5.3f,M,," % (
                     now.hour, now.minute, now.second, self.latDeg, self.latMin, self.flagN,
                     self.lonDeg, self.lonMin, self.flagE, self.height)
        checksum = self.calculateCheckSum(ggaString)
        return "$%s*%s\r\n" % (ggaString, checksum)
    def calculateCheckSum(self, stringToCheck):
        xsum_calc = 0
        for char in stringToCheck:
            xsum_calc = xsum_calc ^ ord(char)
        return "%02X" % xsum_calc
    def get_ID(self):
        '''get ID of last packet'''
        return self.last_id
    def read(self):
        if self.socket is None:
            time.sleep(0.1)
            self.connect()
            return None
        if not self.found_header:
            if not self.sent_header:
                self.sent_header = True
                time.sleep(0.1)
                mps = self.getMountPointString()
                if sys.version_info.major >= 3:
                    mps = bytearray(mps, 'ascii')
                try:
                    self.socket.sendall(mps)
                except Exception:
                    self.socket = None
                    return None
            try:
                casterResponse = self.socket.recv(4096)
            except ssl.SSLWantReadError:
                    return None
            except IOError as e:
                if e.errno == errno.EWOULDBLOCK:
                    return None
                self.socket = None
                casterResponse = ''
            if sys.version_info.major >= 3:
                casterResponse = str(casterResponse, 'ascii')
            header_lines = casterResponse.split("\r\n")
            for line in header_lines:
                if line == "":
                    self.found_header = True
                if line.find("SOURCETABLE") != -1:
                    raise NtripError("Mount point does not exist")
                elif line.find("401 Unauthorized") != -1:
                    raise NtripError("Unauthorized request")
                elif line.find("404 Not Found") != -1:
                    raise NtripError("Mount Point does not exist")
                elif line.find(" 200 OK") != -1:
                    # Request was valid
                    try:
                        gga = self.getGGAString()
                        if sys.version_info.major >= 3:
                            gga = bytearray(gga, 'ascii')
                        self.socket.sendall(gga)
                    except Exception:
                        self.socket = None
                        return None
            return None
        # normal data read
        while True:
            try:
                data = self.socket.recv(1)
            except ssl.SSLWantReadError:
                    return None
            except IOError as e:
                if e.errno == errno.EWOULDBLOCK:
                    return None
                self.socket.close()
                self.socket = None
                return None
            except Exception:
                self.socket.close()
                self.socket = None
                return None
            if len(data) == 0:
                self.socket.close()
                self.socket = None
                return None
            if self.rtcm3.read(data):
                self.last_id = self.rtcm3.get_packet_ID()
                return self.rtcm3.get_packet()
    def connect(self):
        '''connect to NTRIP server'''
        self.sent_header = False
        self.found_header = False
        sock = socket.socket(socket.AF_INET, socket.SOCK_STREAM)
        if self.ssl:
            sock = ssl.wrap_socket(sock)
        try:
            error_indicator = sock.connect_ex((self.caster, self.port))
        except Exception:
            return False
        if error_indicator == 0:
            sock.setblocking(0)
            self.socket = sock
            self.rtcm3.reset()
            return True
        return False
    def readLoop(self):
        while True:
            data = self.read()
            if data is None:
                continue
            ##ADDED
            ser = serial.Serial("/dev/serial0", 115200)
            ser.write(data)
            time.sleep(0.01)
            #
            #print(data)
            print("got: ", len(data))
if __name__ == '__main__':
    usage = "NtripClient.py [options] [caster] [port] mountpoint"
    parser = OptionParser(version=version, usage=usage)
    parser.add_option("-u", "--user", type="string", dest="user", default="IBS", help="The Ntripcaster username.  Default: %default")
    parser.add_option("-p", "--password", type="string", dest="password", default="IBS", help="The Ntripcaster password. Default: %default")
    parser.add_option("-o", "--org", type="string", dest="org", help="Use IBSS and the provided organization for the user. Caster and Port are not needed in this case Default: %default")
    parser.add_option("-b", "--baseorg", type="string", dest="baseorg", help="The org that the base is in. IBSS Only, assumed to be the user org")
    parser.add_option("-t", "--latitude", type="float", dest="lat", default=50.09, help="Your latitude.  Default: %default")
    parser.add_option("-g", "--longitude", type="float", dest="lon", default=8.66, help="Your longitude.  Default: %default")
    parser.add_option("-e", "--height", type="float", dest="height", default=1200, help="Your ellipsoid height.  Default: %default")
    parser.add_option("-s", "--ssl", action="store_true", dest="ssl", default=False, help="Use SSL for the connection")
    parser.add_option("-H", "--host", action="store_true", dest="host", default=False, help="Include host header, should be on for IBSS")
    parser.add_option("-2", "--V2", action="store_true", dest="V2", default=False, help="Make a NTRIP V2 Connection")
    (options, args) = parser.parse_args()
    ntripArgs = {}
    ntripArgs['lat'] = options.lat
    ntripArgs['lon'] = options.lon
    ntripArgs['height'] = options.height
    ntripArgs['host'] = options.host
    ##ADDED
    ntripArgs['user'] = "GRSM:GRSM"
    ntripArgs['caster'] = "ntrip.nps.gov"
    ntripArgs['port'] = 2101
    ntripArgs['mountpoint'] = "GRSM_RTCM3x"
    ##
    n = NtripClient(**ntripArgs)
    n.readLoop()
rtcm3.py
'''Decode RTCM v3 messages'''
RTCMv3_PREAMBLE = 0xD3
POLYCRC24 = 0x1864CFB
import struct
class RTCM3:
    def __init__(self, debug=False):
        self.crc_table = None
        self.debug = debug
        self.reset()
    def get_packet(self):
        '''return bytearray of last parsed packet'''
        return self.parsed_pkt
    def get_packet_ID(self):
        '''get get of packet, or None'''
        if self.parsed_pkt is None or len(self.parsed_pkt) < 8:
            return None
        id, = struct.unpack('>H', self.parsed_pkt[3:5])
        id >>= 4
        return id
    def reset(self):
        '''reset state'''
        self.pkt = bytearray()
        self.pkt_len = 0
        self.parsed_pkt = None
    def parse(self):
        '''parse packet'''
        parity = self.pkt[-3:]
        crc1 = parity[0] << 16 | parity[1] << 8 | parity[2]
        crc2 = self.crc24(self.pkt[:-3])
        if crc1 != crc2:
            if self.debug:
                print("crc fail len=%u" % len(self.pkt))
            # look for preamble
            idx = self.pkt[1:].find(bytearray([RTCMv3_PREAMBLE]))
            if idx >= 0:
                self.pkt = self.pkt[1+idx:]
                if len(self.pkt) >= 3:
                    self.pkt_len, = struct.unpack('>H', self.pkt[1:3])
                    self.pkt_len &= 0x3ff
                else:
                    self.pkt_len = 0
            else:
                self.reset()
            return False
        # got a good packet
        self.parsed_pkt = self.pkt
        self.pkt = bytearray()
        self.pkt_len = 0
        return True
    def read(self, byte):
        '''read in one byte, return true if a full packet is available'''
        #import random
        #if random.uniform(0,1000) < 1:
        #    return False
        byte = ord(byte)
        if len(self.pkt) == 0 and byte != RTCMv3_PREAMBLE:
            # discard
            return False
        self.pkt.append(byte)
        if self.pkt_len == 0 and len(self.pkt) >= 3:
            self.pkt_len, = struct.unpack('>H', self.pkt[1:3])
            self.pkt_len &= 0x3ff
            if self.pkt_len == 0:
                self.reset()
                return False
        if self.pkt_len > 0 and len(self.pkt) >= 3 + self.pkt_len + 3:
            remainder = self.pkt[6+self.pkt_len:]
            self.pkt = self.pkt[:6+self.pkt_len]
            # got header, packet body and parity
            ret = self.parse()
            self.pkt.extend(remainder)
            return ret
        # need more bytes
        return False
    def crc24(self, bytes):
        '''calculate 24 bit crc'''
        if self.crc_table is None:
            # initialise table
            self.crc_table = [0] * 256
            for i in range(256):
                self.crc_table[i] = i<<16
                for j in range(8):
                    self.crc_table[i] <<= 1
                    if (self.crc_table[i] & 0x1000000):
                        self.crc_table[i] ^= POLYCRC24
        crc = 0
        for b in bytes:
            crc = ((crc<<8)&0xFFFFFF) ^ self.crc_table[(crc>>16) ^ b]
        return crc
if __name__ == '__main__':
    from argparse import ArgumentParser
    import time
    parser = ArgumentParser(description='RTCM3 parser')
    parser.add_argument("filename", type=str, help="input file")
    parser.add_argument("--debug", action='store_true', help="show errors")
    parser.add_argument("--follow", action='store_true', help="continue reading on EOF")
    args = parser.parse_args()
    rtcm3 = RTCM3(args.debug)
    f = open(args.filename, 'rb')
    while True:
        b = f.read(1)
        if len(b) == 0:
            if args.follow:
                time.sleep(0.1)
                continue
            break
        if rtcm3.read(b):
            print("packet len %u ID %u" % (len(rtcm3.get_packet()), rtcm3.get_packet_ID()))