Interference with two bus masters on i2c

I am using the “waveshare general driver for robots” which incorporates an esp32, motor controller, IMU and a few other things. And it is designed with a 40 pin connector so that I can serve as a “hat” for a raspberry Pi.

But there’s what I would consider a “defect” to the board. They pass through the two i2c pins from the esp32 to the raspberry pi 40 pin connector using the default 2 (or 4 depending on how you count) pins for the i2c. If you write code on the Pi to use i2C you end up having two i2c bus masters which is never allowed so this is not useful and worse, interferes with using i2c on the pi.

I can think of two ways to address this: either don’t attach the general driver board directly to the Pi. The only other pins that are live are the 5v/gnd pins. The esp32 itself is connected via a separate USB. So I can power the pi with a conventional usb supply. The other is to use what I read is called “software i2c” - bit banging (?) to reassign the two i2c pins (which I read my affect performance, but no idea if that’s true.)

You could cut the traces on your board to disconnect I2C between the pi and board. A little jumper wire could reconnect them in the future if you needed to reconnect them later.

1 Like

The other thing you could do, if you are able to reprogram the ESP32, is to make the ESP to be an I2C slave by passing in an address when you call Wire.begin(). That way the pi can be the sole master.

Why do you say two I2C bus masters is never allowed? The I2C spec permits clock stretching and arbitration for the sole purpose of of allowing two masters to operate on the same bus. Is this an operational constraint placed on the board you’re trying to use? If it isn’t, it may just be a matter of ensuring the Pi and your ESP32 board are configured as multimasters.

Well, in doing some more research, it seems like the Pi may be the limiting factor. I’m not as familiar with the Raspberry Pi, but it seems that its processor only supports single master I2C operation. I guess I learned something new today!

1 Like

Maybe this is an example that can be used: GitHub - waveshareteam/ugv_rpi: Raspberry Pi example for the WaveShare UGV robots: WAVE ROVER, UGV Rover, UGV Beast, RaspRover, UGV01, UGV02.