I purchased an antenna item number GPS-14986 which arrived a couple of days ago. I connected to my UBlox MAX8-based GPS system which provides 3.2V power to the antenna. The system runs for maybe 4 hours and then I get no reception. I have tried bending the wire at various points but I can’t associate such movements with the antenna working/not working. I have another antenna that I can substitute for the GPS-14986 and the substitute antenna runs with no issues.
I’m pretty certain that there is an intermittent fault with the GPS-14986 I received and wish to have the item replaced.