After reading all the forum I found about my problem, I am asking help ! I would like to trigger an interrupt on timer0 every 10 ms and it doesn’t work at all ! Maybe it comes from the Startup file but I have no idea where !
Here is my code :
Startup.S
/***********************************************************************/
/* This file is part of the uVision/ARM development tools */
/* Copyright KEIL ELEKTRONIK GmbH 2002-2005 */
/***********************************************************************/
/* */
/* STARTUP.S: Startup file for Philips LPC2000 device series */
/* */
/***********************************************************************/
/*
This file has been heavily modified for the GNU-Toolchain by:
Martin Thomas, Kaiserslautern, Germany
<mthomas@rhrk.uni-kl.de>
http://www.siwawi.arubi.uni-kl.de/avr_projects
If it does not work for you: don't blame Keil or Philips.
*/
/*
//*** <<< Use Configuration Wizard in Context Menu >>> ***
*/
/*
* The STARTUP.S code is executed after CPU Reset. This file may be
* translated with the following SET symbols. In uVision these SET
* symbols are entered under Options - ASM - Set.
*
* REMAP: when set the startup code initializes the register MEMMAP
* which overwrites the settings of the CPU configuration pins. The
* startup and interrupt vectors are remapped from:
* 0x00000000 default setting (not remapped)
* 0x80000000 when EXTMEM_MODE is used
* 0x40000000 when RAM_MODE is used
*
* EXTMEM_MODE: when set the device is configured for code execution
* from external memory starting at address 0x80000000. The startup
* vectors are located to 0x80000000.
*
* RAM_MODE: when set the device is configured for code execution
* from on-chip RAM starting at address 0x40000000. The startup
* vectors are located to 0x40000000.
*/
/* Map Preprocessor definitions to assembler definitions/symbols */
.set EXTMEM_MODE, 0
#ifdef ROM_RUN
.set RAM_MODE, 0
#ifdef VECTORS_IN_RAM
.set REMAP, 1
.set VECTREMAPPED, 1
#else
.set REMAP, 0
.set VECTREMAPPED, 0
#endif
#endif
#ifdef RAM_RUN
.set RAM_MODE, 1
.set REMAP, 1
.set VECTREMAPPED, 0
#endif
.if (RAM_MODE)
.print "RAM_MODE enabled"
.else
.print "ROM_MODE enabled"
.endif
.if (REMAP)
.print "remapping enabled"
.endif
.if (VECTREMAPPED)
.print "Vectors at start of RAM"
.else
.print "Vectors at start of Code"
.endif
// Standard definitions of Mode bits and Interrupt (I & F) flags in PSRs
.set Mode_USR, 0x10
.set Mode_FIQ, 0x11
.set Mode_IRQ, 0x12
.set Mode_SVC, 0x13
.set Mode_ABT, 0x17
.set Mode_UND, 0x1B
.set Mode_SYS, 0x1F
.set I_Bit, 0x80 /* when I bit is set, IRQ is disabled */
.set F_Bit, 0x40 /* when F bit is set, FIQ is disabled */
/*
// <h> Stack Configuration (Stack Sizes in Bytes)
// <o0> Undefined Mode <0x0-0xFFFFFFFF:4>
// <o1> Supervisor Mode <0x0-0xFFFFFFFF:4>
// <o2> Abort Mode <0x0-0xFFFFFFFF:4>
// <o3> Fast Interrupt Mode <0x0-0xFFFFFFFF:4>
// <o4> Interrupt Mode <0x0-0xFFFFFFFF:4>
// <o5> User/System Mode <0x0-0xFFFFFFFF:4>
// </h>
*/
.set UND_Stack_Size, 0x00000080
.set SVC_Stack_Size, 0x00000080
.set ABT_Stack_Size, 0x00000080
.set FIQ_Stack_Size, 0x00000080
.set IRQ_Stack_Size, 0x00000200
//.set USR_Stack_Size, 0x00000800
.set USR_Stack_Size, 0x00001000
#if 0
AREA STACK, DATA, READWRITE, ALIGN=2
DS (USR_Stack_Size+3)&~3 ; Stack for User/System Mode
DS (SVC_Stack_Size+3)&~3 ; Stack for Supervisor Mode
DS (IRQ_Stack_Size+3)&~3 ; Stack for Interrupt Mode
DS (FIQ_Stack_Size+3)&~3 ; Stack for Fast Interrupt Mode
DS (ABT_Stack_Size+3)&~3 ; Stack for Abort Mode
DS (UND_Stack_Size+3)&~3 ; Stack for Undefined Mode
#endif
.arm
.section .stack, "w"
.align 4
.space (USR_Stack_Size+3)&~3 // Stack for User/System Mode
.space (SVC_Stack_Size+3)&~3 // Stack for Supervisor Mode
.space (IRQ_Stack_Size+3)&~3 // Stack for Interrupt Mode
.space (FIQ_Stack_Size+3)&~3 // Stack for Fast Interrupt Mode
.space (ABT_Stack_Size+3)&~3 // Stack for Abort Mode
.space (UND_Stack_Size+3)&~3 // Stack for Undefined Mode
Top_Stack:
// VPBDIV definitions
.set VPBDIV, 0xE01FC100 /* VPBDIV Address */
/*
// VPBDIV Setup
// Peripheral Bus Clock Rate
// <o1.0..1> VPBDIV: VPB Clock
// <0=> VPB Clock = CPU Clock / 4
// <1=> VPB Clock = CPU Clock
// <2=> VPB Clock = CPU Clock / 2
// <o1.4..5> XCLKDIV: XCLK Pin
// <0=> XCLK Pin = CPU Clock / 4
// <1=> XCLK Pin = CPU Clock
// <2=> XCLK Pin = CPU Clock / 2
//
*/
.set VPBDIV_SETUP, 1
.set VPBDIV_Val, 0x00000000
// Phase Locked Loop (PLL) definitions
.set PLL_BASE, 0xE01FC080 /* PLL Base Address */
.set PLLCON_OFS, 0x00 /* PLL Control Offset*/
.set PLLCFG_OFS, 0x04 /* PLL Configuration Offset */
.set PLLSTAT_OFS, 0x08 /* PLL Status Offset */
.set PLLFEED_OFS, 0x0C /* PLL Feed Offset */
.set PLLCON_PLLE, (1<<0) /* PLL Enable */
.set PLLCON_PLLC, (1<<1) /* PLL Connect */
.set PLLCFG_MSEL, (0x1F<<0) /* PLL Multiplier */
.set PLLCFG_PSEL, (0x03<<5) /* PLL Divider */
.set PLLSTAT_PLOCK, (1<<10) /* PLL Lock Status */
/*
// PLL Setup
// <i> Phase Locked Loop
// <i> CCLK - Processor Clock
// <i> Fcco - PLL Oscillator
// <o1.0..4> MSEL: PLL Multiplier Selection
// <1-32><#-1>
// <i> PLL Multiplier "M" Value
// <i> CCLK = M * Fosc
// <o1.5..6> PSEL: PLL Divider Selection
// <0=> 1 <1=> 2 <2=> 4 <3=> 8
// <i> PLL Divider "P" Value
// <i> Fcco = CCLK * 2 * P
// <i> 156MHz <= Fcco <= 320MHz
//
*/
// .set PLL_SETUP, 1
.set PLLCFG_Val, 0x00000024
// Memory Accelerator Module (MAM) definitions
.set MAM_BASE, 0xE01FC000 /* MAM Base Address */
.set MAMCR_OFS, 0x00 /* MAM Control Offset*/
.set MAMTIM_OFS, 0x04 /* MAM Timing Offset */
/*
// MAM Setup
// <i> Memory Accelerator Module
// <o1.0..1> MAM Control
// <0=> Disabled
// <1=> Partially Enabled
// <2=> Fully Enabled
// <i> Mode
// <o2.0..2> MAM Timing
// <0=> Reserved <1=> 1 <2=> 2 <3=> 3
// <4=> 4 <5=> 5 <6=> 6 <7=> 7
// <i> Fetch Cycles
//
*/
// .set MAM_SETUP, 1
.set MAMCR_Val, 0x00000002
.set MAMTIM_Val, 0x00000004
// Starupt Code must be linked first at Address at which it expects to run.
.if (EXTMEM_MODE)
.set CODE_BASE, 0x80000000
.elseif (RAM_MODE)
.set CODE_BASE, 0x40000000
.else
.set CODE_BASE, 0x00000000
.endif
#if 0
AREA STARTUPCODE, CODE, AT CODE_BASE // READONLY, ALIGN=4
PUBLIC __startup
EXTERN CODE32 (?C?INIT)
__startup PROC CODE32
// Pre-defined interrupt handlers that may be directly
// overwritten by C interrupt functions
EXTERN CODE32 (Undef_Handler?A)
EXTERN CODE32 (SWI_Handler?A)
EXTERN CODE32 (PAbt_Handler?A)
EXTERN CODE32 (DAbt_Handler?A)
EXTERN CODE32 (IRQ_Handler?A)
EXTERN CODE32 (FIQ_Handler?A)
#endif
.text
.arm
.if (VECTREMAPPED)
.print "Vectors in section .vectmapped -> .data"
.section .vectmapped, "ax"
.else
.print "Vectors in section .vectorg -> .text"
.section .vectorg, "ax"
.endif
// Pre-defined interrupt handlers that may be directly
// overwritten by C interrupt functions
.extern Undef_Handler
.extern SWI_Handler
.extern PAbt_Handler
.extern DAbt_Handler
.extern IRQ_Handler
.extern FIQ_Handler
// Exception Vectors
// Mapped to Address 0.
// Absolute addressing mode must be used.
__Vectors: LDR PC,Reset_Addr
LDR PC,Undef_Addr
LDR PC,SWI_Addr
LDR PC,PAbt_Addr
LDR PC,DAbt_Addr
NOP /* Reserved Vector */
LDR PC,[PC, #-0x0FF0] /* Vector from VicVectAddr */
LDR PC,IRQ_Wrapper_Addr
LDR PC,FIQ_Addr
Reset_Addr: .word Reset_Handler
Undef_Addr: .word Undef_Handler
// SWI_Addr: .word SWI_Handler
// SWI_Wrapper_Addr: .word SWI_Wrapper
SWI_Addr: .word 0 /* in swi_handler.S */
PAbt_Addr: .word PAbt_Handler
DAbt_Addr: .word DAbt_Handler
.word 0 /* Reserved Address */
IRQ_Addr: .word IRQ_Handler
IRQ_Wrapper_Addr: .word __IRQ_Wrapper
FIQ_Addr: .word FIQ_Handler
Undef_Handler: B Undef_Handler
/* SWI_Handler: B SWI_Handler */
PAbt_Handler: B PAbt_Handler
DAbt_Handler: B DAbt_Handler
IRQ_Handler: B IRQ_Handler
FIQ_Handler: B FIQ_Handler
.size __Vectors, . - __Vectors
.arm
.section .init, "ax"
.if (VECTREMAPPED)
/* mthomas: Dummy used during startup - mind the nops since the
flash-utility will overwrite the "reserved vector"-address
with the checksum */
B Reset_Handler
NOP
NOP
NOP
NOP
NOP /* Reserved Address */
NOP
NOP
.endif
.arm
.section .init, "ax"
.global __startup
.func __startup
__startup:
Reset_Handler:
// Memory Mapping
.set MEMMAP, 0xE01FC040 /* Memory Mapping Control */
.if (REMAP)
LDR R0, =MEMMAP
.if (EXTMEM_MODE)
MOV R1, #3
.elseif (RAM_MODE) || (VECTREMAPPED)
.print "MEMMAP to 2 on init"
MOV R1, #2
.else
MOV R1, #1
.endif
STR R1, [R0]
.endif
// Setup Stack for each mode
LDR R0, =Top_Stack
// Enter Undefined Instruction Mode and set its Stack Pointer
MSR CPSR_c, #Mode_UND|I_Bit|F_Bit
MOV SP, R0
SUB R0, R0, #UND_Stack_Size
// Enter Abort Mode and set its Stack Pointer
MSR CPSR_c, #Mode_ABT|I_Bit|F_Bit
MOV SP, R0
SUB R0, R0, #ABT_Stack_Size
// Enter FIQ Mode and set its Stack Pointer
MSR CPSR_c, #Mode_FIQ|I_Bit|F_Bit
MOV SP, R0
SUB R0, R0, #FIQ_Stack_Size
// Enter IRQ Mode and set its Stack Pointer
MSR CPSR_c, #Mode_IRQ|I_Bit|F_Bit
MOV SP, R0
SUB R0, R0, #IRQ_Stack_Size
// Enter Supervisor Mode and set its Stack Pointer
MSR CPSR_c, #Mode_SVC|I_Bit|F_Bit
MOV SP, R0
SUB R0, R0, #SVC_Stack_Size
// Enter User Mode and set its Stack Pointer
MSR CPSR_c, #Mode_SYS /* Interrupts enabled */
// MSR CPSR_c, #Mode_USR|I_Bit|F_Bit /* Interrupts disabled */
MOV SP, R0
.if (RAM_MODE==0)
/* Relocate .data section (Copy from ROM to RAM) */
LDR R1, =_etext
LDR R2, =_data
LDR R3, =_edata
CMP R2, R3
BEQ DataIsEmpty
LoopRel: CMP R2, R3
LDRLO R0, [R1], #4
STRLO R0, [R2], #4
BLO LoopRel
DataIsEmpty:
.endif
/* Clear .bss section (Zero init) */
MOV R0, #0
LDR R1, =__bss_start__
LDR R2, =__bss_end__
CMP R1,R2
BEQ BSSIsEmpty
LoopZI: CMP R1, R2
STRLO R0, [R1], #4
BLO LoopZI
BSSIsEmpty:
// call C++ constructors of global objects
LDR r0, =__ctors_start__
LDR r1, =__ctors_end__
ctor_loop:
CMP r0, r1
BEQ ctor_end
LDR r2, [r0], #4
STMFD sp!, {r0-r1}
MOV lr, pc
MOV pc, r2
LDMFD sp!, {r0-r1}
B ctor_loop
ctor_end:
// Enter the C code
//LDR R0,=INIT
LDR R0,=main
TST R0,#1 // Bit-0 set: main is Thumb
LDREQ LR,=__exit_ARM // ARM Mode
LDRNE LR,=__exit_THUMB // Thumb Mode
BX R0
.size __startup, . - __startup
.endfunc
.arm
.global __exit_ARM
.func __exit_ARM
__exit_ARM:
B __exit_ARM
.size __exit_ARM, . - __exit_ARM
.endfunc
.thumb
.global __exit_THUMB
.func __exit_THUMB
__exit_THUMB:
B __exit_THUMB
.size __exit_THUMB, . - __exit_THUMB
.endfunc
/* mthomas: the following code is inspired by various examples and
documents from ARM, Atmel, Anglia Designs and others */
.text
.arm
.if (VECTREMAPPED)
.print "Handlers in section .vectmapped -> .data"
.section .vectmapped, "ax"
.else
.print "Handlers in section .vectorg -> .code/.text"
.section .vectorg, "ax"
.endif
.set VIC_base_addr, 0xFFFFF000
.set VIC_vect_offs, 0x30
.arm
.global __IRQ_Wrapper
.func __IRQ_Wrapper
__IRQ_Wrapper:
/*- Manage Exception Entry */
/*- Adjust and save LR_irq in IRQ stack */
sub lr, lr, #4
stmfd sp!, {lr}
/*- Save SPSR need to be saved for nested interrupt */
mrs r14, SPSR
stmfd sp!, {r14}
/*- Save and r0 in IRQ stack */
stmfd sp!, {r0}
/*- Write in the IVR to support Protect Mode */
/*- No effect in Normal Mode */
/*- De-assert the NIRQ and clear the source in Protect Mode */
/* R14 = LR */
ldr r14, =VIC_base_addr
ldr r0 , [r14, #VIC_vect_offs]
/*str r14, [r14, #VIC_vect_offs]*/
/*- Enable Interrupt and Switch in Supervisor Mode */
msr CPSR_c, #Mode_SVC
/*- Save scratch/used registers and LR in User Stack */
/*stmfd sp!, { r1-r3, r12, r14}*/
stmfd sp!, { r1-r12, r14 }
/*- Branch to the routine pointed by the VIC-Vector-Address */
mov r14, pc
bx r0
/*- Restore scratch/used registers and LR from User Stack*/
/* ldmia sp!, { r1-r3, r12, r14} */
ldmia sp!, { r1-r12, r14 }
/*- Disable Interrupt and switch back in IRQ mode */
msr CPSR_c, #I_Bit | Mode_IRQ
#if 0
/* VICVectAddr=0 is already done in the ISRs of the Philips-Examples
so commented out here */
/*- Mark the End of Interrupt on the VIC */
ldr r14, =VIC_base_addr
str r14, [r14, #VIC_vect_offs]
#endif
/*- Restore SPSR_irq and r0 from IRQ stack */
ldmia sp!, {r0}
/*- Restore SPSR_irq and r0 from IRQ stack */
ldmia sp!, {r14}
msr SPSR_cxsf, r14
/*- Restore adjusted LR_irq from IRQ stack directly in the PC */
ldmia sp!, {pc}^
.size __IRQ_Wrapper, . - __IRQ_Wrapper
.endfunc
#if 0
/* mthomas:
Wrapper to call a C swi-Function declared with
void SWI_Handler(int swi_num, int *regs)
Inspired by Anglia Designs example
-- not used here - see swi_handler.S
*/
.arm
.global __SWI_Wrapper
.func __SWI_Wrapper
__SWI_Wrapper: /* r0 holds swi number */
STMFD sp!,{r0-r12,lr} /* Save The workspace plus the current return */
/* address lr_ mode into the stack */
MRS r1, spsr /* Save the spsr_mode into r1 */
STMFD sp!, {r1} /* Save spsr */
MOV r1, sp /* load regs */
LDR r0,=SWI_Handler
MOV lr, pc
BX r0 /* call the C-funcktion */
LDMFD sp!, {r1} /* Restore the saved spsr_mode into r1 */
MSR spsr_cxsf, r1 /* Restore spsr_mode */
LDMFD sp!, {r0-r12,pc} /* Return to the instruction following */
/* the exception interrupt */
.size __SWI_Wrapper, . - __SWI_Wrapper
.endfunc
#endif
#if 0
/* mthomas: not used here - reminder for future tests */
.arm
.global __IRQ_Wrapper
.func __IRQ_Wrapper
__IRQ_Wrapper:
SUB lr, lr, #4 /* Update the link register */
STMFD sp!,{r0-r12,lr} /* Save The workspace plus the current return */
/* address lr_ mode into the stack */
MRS r1, spsr /* Save the spsr_mode into r1 */
STMFD sp!, {r1} /* Save spsr */
LDR lr, =ReturnAddress /* Read the return address. */
LDR r0, =VIC_base_addr /* Load VIC Base-Address */
LDR r1, [r0, #VIC_vect_offs] /* Load ISR-Address from VICVectAddr */
bx r1 /* Branch to the IRQ handler. */
ReturnAddress:
LDR r2, =VIC_base_addr /* clear Interrupt */
MOV r3, #0
STR R3, [R2, #VIC_vect_offs] /* by writing to VICVectAddr */
LDMFD sp!, {r1} /* Restore the saved spsr_mode into r1 */
MSR spsr_cxsf, r1 /* Restore spsr_mode */
LDMFD sp!, {r0-r12,pc}^ /* Return to the instruction following */
/* the exception interrupt */
.size __IRQ_Wrapper, . - __IRQ_Wrapper
.endfunc
#endif
.end
TIMER0 :
satic unsigned long int tFreq;
void timer0Init(unsigned long int freq)
{
tFreq=freq;
T0PR=Fcclk/tFreq; //Set up the prescaler for a 'freq' frequency
T0CTCR=0; //Timer Mode
T0TCR |=0X01; //Enable the clock
//T0MCR=0x0003; //Interrupt and Reset Timer on Match
//T0MR0=(50000/TIMER_FREQ);
}
void timer0Match(int mr, unsigned long int freq, char mode)
{
unsigned long int mfreq = tFreq/freq; //Get the Match Register value by dividing timer frequency by request match frequency
switch(mr)
{
case 0:
T0MR0 = mfreq;
T0MCR = (mode<<0);
break;
case 1:
T0MR1 = mfreq;
T0MCR = (mode<<3);
break;
case 2:
T0MR2 = mfreq;
T0MCR = (mode<<6);
break;
case 3:
T0MR3 = mfreq;
T0MCR = (mode<<9);
break;
default:
break;
}
}
char timer0IntFlag=0;
long int ms=0;
//Usage: None (Automatically Called by FW)
//Inputs: None
//This function is a global interrupt called by a match on the Timer 0 match.
void ISR_Timer0(void)
{
rprintf("timer0 interrupt\n");
//Interrupt Code Here
timer0IntFlag+=1;
//Keep track of the number of milliseconds
ms++;
//Clear the interrupt and update the VIC priority
T0IR = 0x01;
VICVectAddr =0;
}
MAIN :
//*******************************************************
// Main Code
//*******************************************************
int main (void)
{
//Initialize ARM I/O
bootUp(); //Init. I/O ports, Comm protocols and interrupts
LEDoff();
timer0Init(1000000);
timer0Match(0, 1000, interruptOnMatch | resetOnMatch);
enableIRQ();
while(1);
return 0;
}
//Usage: bootUp();
//Inputs: None
//This function initializes the serial port, the SD card, the I/O pins and the interrupts
void bootUp(void)
{
// initialise FCCLK--------------------
PLLCON = 1; // enable PLL
PLLCFG = (1 << 5) | 4; // P = 2, M = 5
PLLFEED = 0xAA;
PLLFEED = 0x55;
///- I0DIR: GPIO port Direction control Register, it controls the direction of each port pin
///- XBEE module is not used
///- IODIR0 |= (LED| XBEE_EN);
IODIR0 |= LED; ///P0.15 is set as an output
while ((PLLSTAT & (1 << 10)) == 0);
PLLCON = 3; // enable and connect
PLLFEED = 0xAA;
PLLFEED = 0x55;
MAMCR=0x02;
MAMTIM=0x04;
//--------------------------------------
//Initialize UART for RPRINTF
init_serial0(115200);
rprintf_devopen(putc_serial0); //Init rprintf
///- The APB Divider determines the relationship between the processor clock (CCLK) and the
///- clock used by peripheral devices (PCLK).
///- VPBDIV = 1 APB bus clock is the same as the processor clock.
VPBDIV=1; // Set PCLK equal to the System Clock
VICIntSelect = ~(INT_TIMER0);
VICVectCntl0 = 0x20 | 4; //Timer 0 Interrupt
VICVectAddr0 = (unsigned int)ISR_Timer0;
rprintf("boot up\n");
}
I will be very very thankful for any help ![]()