Hello, Need help for 2 problem that y have with this code that y put together , fist problem is that y cant seems to be able to make the (PowerSB Raw code ) to work, all the Oder code are transmitting fine, y suspect it is the length of the Raw code that is a problem,
The second issue that y have is that y not able to repeat a code, if y do a one click it works fine but since this code is for controlling the volume of the SB y want to be able to hold the volume Up or down for the desire level, try to play with delays but it did not do a good job, the code y have doesnt have a repeat FFFFF code
Thanks for your help ![]()
/* translator Remote Control for Samsung Soundbase
.
*/
#include <IRremote.h>
int RECV_PIN = 11;
IRrecv irrecv(RECV_PIN);
decode_results results;
IRsend irsend; //for some reason always on pin 3?
#define Power_TV 3772793023 //E0E040BF
#define Mute_TV 3772837903 //E0E0F00F
#define Volume_Up_TV 3772833823 //E0E0E01F
#define VolumeDown_Tv 3772829743 //E0E0D02F
unsigned int MuteSB[77] = {4700,4200, 700,300, 700,300, 700,300, 700,300, 650,1300, 700,1250, 650,350, 650,350, 650,1300, 650,1300, 650,1300, 650,1300, 650,350, 650,350, 650,350, 650,300, 650,4350, 600,350, 650,350, 650,350, 650,350, 600,1350, 650,350, 600,400, 600,350, 650,1300, 650,1350, 600,1350, 600,400, 600,350, 650,1300, 650,1350, 600,1350, 600,350, 650,350, 650,350, 650,1300, 650};
unsigned int PowerSB[99] = {3650,1500, 650,250, 600,1100, 650,250, 600,250, 600,250, 600,250, 600,250, 650,250, 600,250, 600,250, 600,250, 600,300, 550,300, 550,1150, 600,250, 600,300, 550,300, 550,300, 600,250, 600,250, 600,300, 550,300, 550,300, 550,1150, 600,300, 550,300, 550,300, 550,300, 550,350, 550,300, 550,300, 550,300, 550,1200, 550,300, 550,1150, 550,1200, 550,1150, 550,1150, 600,300, 550,300, 550,1150, 550,350, 550,1150, 550,1150, 550,1200, 550,1150, 550,350, 500,1200, 550};
unsigned int VolumeUp[77] = {4700,4200, 750,300, 650,300, 700,300, 700,300, 650,1300, 700,1250, 700,300, 650,350, 650,1250, 700,1300, 650,1300, 650,1300, 650,350, 650,350, 650,350, 650,300, 650,4300, 650,350, 650,350, 650,350, 650,350, 600,1350, 600,1350, 600,1350, 650,350, 600,1350, 600,1350, 600,1350, 650,350, 600,400, 600,400, 600,350, 650,1300, 650,350, 650,350, 600,400, 600,1350, 600};
unsigned int VolumeDown[77] = {4650,4250, 700,300, 700,300, 700,300, 650,350, 650,1300, 650,1300, 650,350, 650,350, 650,1300, 650,1300, 650,1300, 650,1300, 650,350, 600,400, 600,350, 650,350, 650,4300, 650,350, 650,350, 600,400, 600,350, 650,350, 650,400, 600,350, 600,1350, 600,1400, 600,1350, 600,1350, 600,400, 600,1350, 600,1350, 600,1350, 600,400, 600,350, 600,400, 600,400, 600,1350, 600};
void setup()
{
irrecv.enableIRIn(); // Start the receiver
irrecv.blink13(1);
}
void loop() {
if (irrecv.decode(&results)) {
delay(4);
switch (results.value) {
case Power_TV:
//Do this when the middle button is pressed
irsend.sendRaw(PowerSB,99,48);
irrecv.enableIRIn();
break;
case Volume_Up_TV:
irsend.sendRaw(VolumeUp,77,32);
irrecv.enableIRIn(); // because irsend disables irrecv
break;
case Mute_TV:
irsend.sendRaw(MuteSB,77,32);
irrecv.enableIRIn(); // because irsend disables irrecv
break;
case VolumeDown_Tv :
irsend.sendRaw(VolumeDown,77,32);
irrecv.enableIRIn(); // because irsend disables irrecv
break;
}
irrecv.resume();
}
}