Is it possible to connect Myoware to custom printed electrodes?

Hi,
I want to know if it is possible to connect the Myoware instrumentation to other type of electrodes, different to those that are in the kit.

If it is possible, have I to solder the electrode cables to the electrodes of mine?

Kind regards

I’ve seen folks use other electrodes…make sure they are equal length cables and that you don’t introduce a ton of resistance with bad junctions and whatnot - what do you mean by 3D printed? Are you try to use conductive filament? Because I doubt that’d work reliably

Thanks for the answer.
No, not 3d printed electrodes but with other methods.
The electrodes are flexible and printed on a flexible substrate. I can connect them to a PCB. From that device I want to create the connection with the Myoware cables.
As you say, this is possible, doesn’t it?

Sure…just be aware of the caveats above (junction noise, etc)