ISL29125 color values always at 0 or max value

Hi! I am using the ISL29125 color sensor, but I haven’t been able to get any expected results. I downloaded this library (GitHub - sparkfun/SparkFun_ISL29125_Breakout_Arduino_Library: Arduino Library and example code for the ISL29125), and I am only trying to run the example code in ISL29125Basics.ino. I added some Serial.print commands to check the state of some things, and even though the init() function works, I always get color values that are either 0 or 65535 (the maximum value).
For extra context, I am using this sensor in an Alphabot2-Ar robot, which uses a board similar to Arduino UNO: the Waveshare R3 PLUS. I am using a logic level converter, and connected everything as is explained in this video https://www.youtube.com/watch?app=desktop&v=MwdANEcTiPY&t=0s&ab_channel=DroneBotWorkshop.

Am I doing something wrong, or did I maybe get a faulty sensor? Is there any way for me to check if it is working correctly?

EDIT: Just to discard some variables, I went to get an Arduino UNO (in the back it says the model is R3), that is not connected to anything else, and it still gave the same values. Although at first the init() was not working, but after I added the following code that only tries to find devices, it started working (I don’t really know why):

  Wire.begin();

  byte error, address;
  int nDevices = 0;

  for (address = 1; address < 127; address++) {
    Wire.beginTransmission(address);
    error = Wire.endTransmission();

    if (error == 0) {
      Serial.print("I2C device found at 0x");
      Serial.println(address, HEX);
      nDevices++;
    }
  }

  if (nDevices == 0)
    Serial.println("No I2C devices found");
    

Does beginning a transmission to the address help it in the init()? This is the init code:

bool SFE_ISL29125::init()
{
  bool ret = true;
  uint8_t data = 0x00;

  // Start I2C
  Wire.begin();

  // Check device ID
  data = read8(DEVICE_ID);
  if (data != 0x7D)
  {
    ret &= false;
  }

  // Reset registers
  ret &= reset();

  // Set to RGB mode, 10k lux, and high IR compensation
  ret &= config(CFG1_MODE_RGB | CFG1_10KLUX, CFG2_IR_ADJUST_HIGH, CFG_DEFAULT);

  return ret;
}

// Reset all registers - returns true if successful
bool SFE_ISL29125::reset()
{
  uint8_t data = 0x00;
  // Reset registers
  write8(DEVICE_ID, 0x46);
  // Check reset
  data = read8(CONFIG_1);
  data |= read8(CONFIG_2);
  data |= read8(CONFIG_3);
  data |= read8(STATUS);
  if (data != 0x00)
  {
    return false;
  }
  return true;
}

The sensor has i2c pull up resistors, ensure your board and the logic converter don’t also have pull ups active (only one set should be used per bus)

The Wire.begin() call must occur before sensor initialization.. adding the I2C device scan likely resolved this by implicitly initializing the I2C bus, being sure to to Wire.Begin before RGB_sensor.init()

It might help to share a photo of your setup/wiring/soldering. Also confirm the voltage levels being delivered to the sensor are good (3.3v, continuity)

Are you using it in a very bright environment?

Hi, thank you for the response. It ended up being just poor connection from my cables because I hadn’t soldered them in place, so they had space to move and create brownout. I only found this after using the readStatus() function, and checking with the datasheet what it meant.