I have quite a bit of experience with the GM862-GPS platform, so i took the plunge, and had two GE863-GPS boards made up.
I am able to get on both modules, and everything appears to work fine. I have performed a couple test calls, etc.
However, the GPS on both of them is acting strangely. When I issue these two commands, i get back a blank response:
AT$GPSACP
$GPSACP:
AT$GPSSW
$GPSSW:
Checking the current consumption, however, gives me an expected value:
AT$GPSAI?
$GPSAI: 9
I suspected that perhaps, maybe, telit’s initial firmware load broke. But after uploading firmware twice on one module, and noticing the other module is acting the same, I have confirmed we are doing something wrong.
The GPS power is turned on, the power save is off (full mode activated), and pretty much all the defaults are in place. Usually on a telit module, at least the 862-GPS, plugging in a GPS antenna and leaving it in a default mode gives you a fix right off the bat—or at the very least–no fix data and the current internal time of the GPS receiver.
I do not think there is an issue with the GPS antenna physically or the wiring because a GM862-GPS will at least give you internal time and invalid fix data without an antenna connected.
I am not using a camera, or doing anything unusual.
any ideas?