Hi!
I have a problem with Olimex JTAG, UART and Timers. When I disconnect JTAG everything works fine and I can use the UART and Timers, but when i debug with JTAG (or the JTAG i physically connected) and click “GO” only junk characters are transmitted. (It’s not enough to stop debugging. I have to remove the cable)
I have an RC servo controlled with PWM, and it only works if I disconnect the JTAG.
What is wrong?
I use a Atmega32 and tried with different boards and different JTAGs.
I tried with internal 1 mhz and external 4 Mhz crystal (15pF).