I’ve come to a particular stage of a project, and with horror I realise I’m going to have to use an ADC. I try to avoid the analogue world where possible ![]()
I’ve only really played around with ADCs on breadboard(!) which is about as non-ideal as you can get - you probably won’t be surprised to hear that the readings were as noisy as anything.
Do I have the general right end of the stick if I do the following on my PCB, which will be 2 layer:
-
Ground plane under the ADC.
-
Decoupling for the ADC supply pins: a couple of 0.1uF multilayer ceramics in parallel.
-
Upstream of this, a choke to reduce supply noise reaching the ADC.
-
Short traces to the connector that goes out to the shielded cable.
The signal to be sampled is very low frequency (changing at less than 1Hz), so I could also add a low pass filter to the analogue inputs and also average the inputs over a period of two or three seconds, but I’d like to get the best performance possible out of the ADC in the first place.
The ADC itself is free-from-the-parts-bin (i.e. a salvage from redundant kit!) in a DIP package, an ADC0803 if memory serves (I don’t have it right in front of me but I’m pretty sure I remember it correctly).