Hi,
I am trying to use the code from the LED Cloud-Connected Cloud in another project that will have the same functions as the LED cloud but will be in the form of an LED matrix instead. I have been able to get it all to work with the exception of the weather portion. The “RGB” and “Disco” buttons work as they should but when I select the “Weather” button in the Blynk app, I receive a “Weather Error” that prints on the Blynk LCD. I receive this error without changing anything in the code provided in the Github repo for this project as well as when I have used my own latitude & longitude and API key from Openweathermap.org. I am using the same components that are listed in the tutorial and everything is wired the same. The only difference between the tutorial and my project is the number of LEDS.
Below is the url for the tutorial I am referring to and the code I currently have uploaded that contains my API and location info.
I feel as though this is some small error, what am I missing?
https://learn.sparkfun.com/tutorials/le … cted-cloud
/**
 * CloudCloud
 * Shawn Hymel @ SparkFun Electronics
 * September 17, 2015
 *
 * Use Blynk app to set up some buttons and LEDs. See the pin
 * definitions below.
 * 
 * 
https://learn.sparkfun.com/tutorials/led-cloud-connected-cloud?_ga=2.158340602.1930760920.1604702820-1392400980.1551950603#electronics-assembly-part-2
 
 * 
 */
#include <ESP8266WiFi.h>
#include <BlynkSimpleEsp8266.h>
#include "States.h"
// Debug to Blynk Serial
#if DEBUG
#define BLYNK_PRINT Serial
#endif
// Pin definitions
#define LED_PIN           5
#define WEATHER_BTN_PIN   V0
#define WEATHER_LED_PIN   V1
#define RGB_BTN_PIN       V2
#define RGB_LED_PIN       V3
#define DISCO_BTN_PIN     V4
#define DISCO_LED_PIN     V5
#define ZERGBA_PIN        V8
#define LCD_PIN           V9
// WiFi parameters
const char WIFI_SSID[] = "ATT3Jz7CFG";
const char WIFI_PSK[] = "9pe+2tfk5757";
const char BLYNK_AUTH[] = "6InHkofnaQ60GusAOz3bOcBOsCV35kJW";
// Other constants
const byte SERIAL_SOF = 0xA5;
const byte SERIAL_EOF = 0x5A;
const int OUT_BUF_MAX = 7;         // bytes
const byte COMM_RGB = 1;
const byte COMM_DISCO = 2;
const byte COMM_BLUE_SKY = 3;
const byte COMM_NIGHT = 4;
const byte COMM_OVERCAST = 5;
const byte COMM_GOLDEN = 6;
const byte COMM_SNOW = 7;
const byte COMM_LIGHTNING = 8;
// Location data (DOWNERS GROVE, IL)
const float LATITUDE = 41.8089;
const float LONGITUDE = -88.0112;
// Remote site information    "api.openweathermap.org/data/2.5/weather?lat=41.8089&lon=-88.0112&appid=11ebc16e8fafb74049b1c02bafdcc1de";
const char http_site[] = "api.openweathermap.org";
const int http_port = 80;
// Other constants
const int TIMEOUT = 300;    // ms
const int BUFFER_SIZE = 22; // bytes
const int ICON_SIZE = 4;    // bytes
const int DT_SIZE = 12;     // bytes
// Global variables
WidgetLED weather_led(WEATHER_LED_PIN);
WidgetLED rgb_led(RGB_LED_PIN);
WidgetLED disco_led(DISCO_LED_PIN);
WidgetLCD lcd(LCD_PIN);
CloudState cloud_state;
WiFiClient client;
WeatherType current_weather;
unsigned long timestamp;
bool force_update;
uint8_t color_r;
uint8_t color_g;
uint8_t color_b;
byte out_msg[OUT_BUF_MAX];
/****************************************************************
 * Setup
 ***************************************************************/
void setup() {
  
  uint8_t led = 0;
  // Set up status LED
  pinMode(LED_PIN, OUTPUT);
  
  // Set up debug serial console
  Serial.begin(9600);
  // Start Blynk and wait for connection
  Blynk.begin(BLYNK_AUTH, WIFI_SSID, WIFI_PSK);
  while ( Blynk.connect() == false ) {
    led ^= 0x01;
    digitalWrite(LED_PIN, led);
    delay(200);
  }
  digitalWrite(LED_PIN, HIGH);
  
  // Define initial state
  cloud_state = CLOUD_WEATHER;
  setLEDs();
  timestamp = millis();
  force_update == false;
  color_r = 0;
  color_g = 0;
  color_b = 0;
  lcd.clear();
}
/****************************************************************
 * Loop
 ***************************************************************/
void loop() {
  Blynk.run();
  
  // Perform LED functions
  switch ( cloud_state ) {
    
    // Reflect weather data in clouds
    case CLOUD_WEATHER:
      doWeather();
      break;
      
    case CLOUD_RGB:
    case CLOUD_DISCO:
    default:
      break;
  }
}
/****************************************************************
 * Blynk Callbacks
 ***************************************************************/
// Callback when weather button is pushed
BLYNK_WRITE(WEATHER_BTN_PIN) {
  if ( (param.asInt() == 1) && (cloud_state != CLOUD_WEATHER) ) {
    cloud_state = CLOUD_WEATHER;
    setLEDs();
    force_update = true;
  }
}
// Callback when RGB button is pushed
BLYNK_WRITE(RGB_BTN_PIN) {
  if ( (param.asInt() == 1) && (cloud_state != CLOUD_RGB) ) {
    cloud_state = CLOUD_RGB;
    setLEDs();
    sendRGB();
  }
}
// Callback when Disco button is pushed
BLYNK_WRITE(DISCO_BTN_PIN) {
  if ( (param.asInt() == 1) && (cloud_state != CLOUD_DISCO) ) {
    cloud_state = CLOUD_DISCO;
    setLEDs();
    sendDisco();
  }
}
// Callback when the ZeRGBa changes
BLYNK_WRITE(ZERGBA_PIN) {
  color_r = param[0].asInt();
  color_g = param[1].asInt();
  color_b = param[2].asInt();
  if ( cloud_state == CLOUD_RGB ) {
    sendRGB();
  }
}
// Set app LEDs
void setLEDs() {
  
  // Turn them all off
  weather_led.off();
  rgb_led.off();
  disco_led.off();
  lcd.clear();
  
  // Only turn on the one we want
  switch ( cloud_state ) {
    case CLOUD_WEATHER:
      weather_led.on();
      lcd.print(0, 0, "WEATHER");
      break;
    case CLOUD_RGB:
      rgb_led.on();
      lcd.print(0, 0, "RGB");
      break;
    case CLOUD_DISCO:
      disco_led.on();
      lcd.print(0, 0, "DISCO");
      break;
    default:
      break;
  }
}
/****************************************************************
 * Send Modes to Pro Mini
 ***************************************************************/
// Send RGB code with red, green, blue values
void sendRGB() {
  out_msg[0] = COMM_RGB;
  out_msg[1] = color_r;
  out_msg[2] = color_g;
  out_msg[3] = color_b;
  transmitMessage(out_msg, 4);
}
// Send Disco code
void sendDisco() {
  out_msg[0] = COMM_DISCO;
  transmitMessage(out_msg, 4);
}
/****************************************************************
 * Weather Functions
 ***************************************************************/
// Every 30 seconds, pull weather data and update LEDs
void doWeather() {
  
  // Only update every 30 seconds
  if ( ((millis() - timestamp) >= 30000) || force_update ) {
    force_update = false;
    timestamp = millis();
    lcd.clear();
    lcd.print(0, 0, "WEATHER");
    
    // Get weather data
    current_weather = getWeather();
  
    // Display weather on clouds
    switch ( current_weather ) {
    
      // Cannot get weather data
      case WEATHER_ERROR:
        lcd.print(0, 1, "ERROR");
        break;
      
      // Clear skies (day)
      case WEATHER_BLUE_SKY:
        lcd.print(0, 1, "BLUE SKY");
        out_msg[0] = COMM_BLUE_SKY;
        break;
      
      // Clear skies (night)
      case WEATHER_NIGHT:
        lcd.print(0, 1, "NIGHT");
        out_msg[0] = COMM_NIGHT;
        break;
      
      // Lots of clouds
      case WEATHER_OVERCAST:
        lcd.print(0, 1, "OVERCAST");
        out_msg[0] = COMM_OVERCAST;
        break;
      
      // Dawn or dusk
      case WEATHER_GOLDEN:
        lcd.print(0, 1, "GOLDEN");
        out_msg[0] = COMM_GOLDEN;
        break;
      
      // It's snowing!
      case WEATHER_SNOW:
        lcd.print(0, 1, "SNOW");
        out_msg[0] = COMM_SNOW;
        break;
      
      // Storm
      case WEATHER_LIGHTNING:
        lcd.print(0, 1, "STORM");
        out_msg[0] = COMM_LIGHTNING;
        break;
      
      // Unknown weather type
      case WEATHER_UNKNOWN:
      default:
        lcd.print(0, 1, "UNKNOWN");
        break;
    }
    transmitMessage(out_msg, 4);
  }
}
// Perform an HTTP GET request to openweathermap.org
WeatherType getWeather() {
  
  unsigned long time = millis();
  unsigned long dt = 0;
  unsigned long sunrise = 0;
  unsigned long sunset = 0;
  char buf[BUFFER_SIZE];
  char icon[ICON_SIZE];
  char dt_str[DT_SIZE];
  char c;
  char* dummy;
  bool golden = false;
  ParserState parser_state = PARSER_START;
  WeatherType condition = WEATHER_UNKNOWN;
  
  // Flush read buffer
  if ( client.available() ) {
    client.read();
  }
  
  // Set string buffers to null
  memset(icon, 0, ICON_SIZE);
  memset(dt_str, 0, DT_SIZE);
  
  // Attempt to make a connection to the remote server
  if ( !client.connect(http_site, http_port) ) {
    return WEATHER_ERROR;
  }
  
  // Construct HTTP GET request
  String cmd = "GET /data/2.5/weather?lat=";
  cmd += String(LATITUDE);
  cmd += "&lon=";
  cmd += String(LONGITUDE);
  cmd += "4c98a1e9b74baa7e105b0d185eac5c81";  //API key from openweathermap.org
  cmd += " HTTP/1.1\nHost: ";
  cmd += http_site;
  cmd += "\nConnection: close\n\n";
  
  // Send out GET request to site
  client.print(cmd);
  
  // Parse data
  while ( (millis() - time) < TIMEOUT ) {
    
    // Get web page data and push to window buffer
    if ( client.available() ) {
      c = client.read();
      pushOnBuffer(c, buf, BUFFER_SIZE);
      time = millis();
    }
    
    // Depending on the state of the parser, look for string
    switch ( parser_state ) {
      case PARSER_START:
        if ( memcmp(buf, "\"weather\":", 10) == 0 ) {
          parser_state = PARSER_WEATHER;
        }
        break;
        
      case PARSER_WEATHER:
        if ( memcmp(buf, "\"icon\":\"", 8) == 0 ) {
          parser_state = PARSER_DT;
          memcpy(icon, buf + 8, 3);
        }
        break;
        
      case PARSER_DT:
        if ( memcmp(buf, "\"dt\":", 5) == 0 ) {
          parser_state = PARSER_SUNRISE;
          memcpy(dt_str, buf + 5, 10); // This assumes 10 digits!
          dt = strtol(dt_str, &dummy, 10);
        }
        break;
        
      case PARSER_SUNRISE:
        if ( memcmp(buf, "\"sunrise\":", 10) == 0 ) {
          parser_state = PARSER_SUNSET;
          memcpy(dt_str, buf + 10, 10); // Assumes 10 digits!
          sunrise = strtol(dt_str, &dummy, 10);
        }
        break;
        
        case PARSER_SUNSET:
        if ( memcmp(buf, "\"sunset\":", 9) == 0 ) {
          parser_state = PARSER_SUNSET;
          memcpy(dt_str, buf + 9, 10); // Assumes 10 digits!
          sunset = strtol(dt_str, &dummy, 10);
        }
        break;
        
      default:
        break;
    }
  }
  
  // Make sure we have a legitimate icon and times
  if ( (strcmp(icon, "") == 0) || (dt == 0) || 
        (sunrise == 0) || (sunset == 0) ) {
    return WEATHER_ERROR;
  }
  
  // See if we are in the golden hour
  if ( ((dt - sunrise) >= 0) && ((dt - sunrise) <= 1800) ) {
    golden = true;
  }
  if ( ((sunset - dt) >= 0) && ((sunset - dt) <= 1800) ) {
    golden = true;
  }
  
  // Lookup what to display based on icon
  // http://openweathermap.org/weather-conditions
  if ( (strcmp(icon, "01d") == 0) || 
        (strcmp(icon, "02d") == 0) ) {
    if ( golden ) {
      return WEATHER_GOLDEN;
    } else {
      return WEATHER_BLUE_SKY;
    }
  } else if ( (strcmp(icon, "01n") == 0) || 
              (strcmp(icon, "02n") == 0) ) {
    if ( golden ) {
      return WEATHER_GOLDEN;
    } else {
      return WEATHER_NIGHT;
    }
  } else if ( (strcmp(icon, "03d") == 0) || 
              (strcmp(icon, "03n") == 0) ||
              (strcmp(icon, "04d") == 0) ||
              (strcmp(icon, "04n") == 0) ||
              (strcmp(icon, "09d") == 0) ||
              (strcmp(icon, "09n") == 0) ||
              (strcmp(icon, "10d") == 0) ||
              (strcmp(icon, "10n") == 0) ) {
    return WEATHER_OVERCAST;
  } else if ( (strcmp(icon, "11d") == 0) ||
              (strcmp(icon, "11n") == 0) ) {
    return WEATHER_LIGHTNING;
  } else if ( (strcmp(icon, "13d") == 0) ||
              (strcmp(icon, "13n") == 0) ) {
    return WEATHER_SNOW;
  } else if ( (strcmp(icon, "50d") == 0) ||
              (strcmp(icon, "50n") == 0) ) {
    return WEATHER_OVERCAST;
  } else {
    return WEATHER_UNKNOWN;
  }
}
// Shift buffer to the left by 1 and append new char at end
void pushOnBuffer(char c, char *buf, uint8_t len) {
  for ( uint8_t i = 0; i < len - 1; i++ ) {
    buf[i] = buf[i + 1];
  }
  buf[len - 1] = c;
}
/****************************************************************
 * Transmitter
 ***************************************************************/
void transmitMessage(byte msg[], uint8_t len) {
  
  int i;
  byte cs;
  byte *out_buf;
  uint8_t buf_size;
  
  // If message is greater than max size, only xmit max bytes
  if ( len > OUT_BUF_MAX ) {
    len = OUT_BUF_MAX;
  }
  
  // Full buffer is message + SOF, EOF bytes
  buf_size = len + 2;
  
  // Create the output buffer with BEGIN, SOF, CS, and EOF
  out_buf = (byte*)malloc(buf_size * sizeof(byte));
  out_buf[0] = SERIAL_SOF;
  memcpy(out_buf + 1, msg, len);
  out_buf[buf_size - 1] = SERIAL_EOF;
  
  // Transmit buffer
  for ( i = 0; i < buf_size; i++ ) {
    Serial.write(out_buf[i]);
  }
  
  // Free some memory
  free(out_buf);
}