We are using a blue LED in our design From Rohm and We have been having premature LED failure within a month from the field. I am not sure what’s going with the LED driver. I have attached the driver circuit/datasheet for your review and help would be greatly appreciated.
Hi, I am working on a design that uses a relay to control LED lights. The schematic shows +12VDC LEDs connected to the (+) terminals, while the other end (-) of the terminal is connected to both an opto-coupler and the relay, which then feeds into the MCU. Regardless of whether the relay is on or off, I only see a high signal at the opto-coupler output. I’m not sure what the issue is with the attached circuit. Can anyone help me identify and rectify the problem? I have already designed a PCB with this circuit and would like to avoid repeating the same mistake in the new build. Thank you