hey i have a ? on an led tv i have found the board which powers the leds, on this board it says led1- led2- nc led+. led3- led4- nc led+. ok, where this comes out of the driver board into the leds, starting with led1- through 4 would it be feasible to install diodes say 1/4 watt inline to each, to prevent voltage feed back into the original circuit. and inject a predetermined current to turn up the brightness on the led strips. say with a pot. we are only dealing with ma. obviously i would run the unit under test to determine its current ma usage. would this not prevent original board damage. of course i would find out the current ratings of the led strips used in this set and stay well under it’s max. hypothetical if rated at 100 ma and using 25, could i not inject say 50 more ma safely.
thanks dboe