if anyone has the PCB design for dimming control on LED, which must adjust the current not voltage.
Can you provide more details of your need?pmacpeter:
if anyone has the PCB design for dimming control on LED, which must adjust the current not voltage.
Hint:
Physical size of PCB required
Number and type of LEDs
Range of current adjustment required
Connection of LEDs (series or parallel)
Number of LEDs in a series chain
Type of supply voltage (AC/DC low voltage, house current)
Number of channels
Type of user control(s)
Are willing to cover the cost of circuit design, PCB design,
PCB fabrication, and shipping?
The PCB will be 2.5 x 2.5 inches.
The LED will be 1 Watt to 100 Watt, if there is limitation on wattage, like must be above 10 Watt, etc.
The range of current adjustment will depend on the total max power
It would be in series connection.
The number of LEDs in a series chain will depend on total max power
The input is 100 to 250V AC
The number of channels will depend on the total max power
Type of user control(s) will be local touch and/or wireless RF
Yes we do
100 watt LED?
Hell, a 10 watt lightbulb can cause eye damage, are you trying to signal god? Message other planets?
I’m developing similar circuit right now. Couple things are different though. First, given 3.7V forward voltage, 100W single string of 1W LEDs would have (surprise!) 370V on it’s ends. If you go with 3W LEDs it would be 120V, which is not that bad but still. Usually for this kind of power you want like 3 strings on separate controllers, this way if one LED dies you’ll still have some light. Second, current adjustment is a bad idea - LED spectrum depends on current, white LED, for example, would look rather blue powered by low current. The right way to control LED intensity is PWM. There is plenty of PWM LED controllers, I prefer ones from Linear Tech.
Shifted:
100 watt LED?
FYI, you can get 100W LEDS…
Here’s one made by Edison Opto: http://www.edison-opto.com.tw/products_ … =1&cno=253
They cost a little bit tho… ![]()
This is not a single LED, it’s a string. Look at rated Vf, it’s 33V:-).
I know, i didn’t say it was a single die product…
Nevermind.
You are not ready to engineer a product with such sloppypmacpeter:
The range of current adjustment will depend on the total max powerThe number of LEDs in a series chain will depend on total max power
The number of channels will depend on the total max power
specs. Are you serious? Are you willing to put ten grand
(USD) on the table to work on your POC prototype?