LiPo powered Artemis Nano

Hi,

I am trying to power my Nano for a mobile project with a 3.7V 1000mAh battery. When connected to USB-C my project draws 13mAh, and thus I figured this would work. However once I switch over to battery the Nano output is on 2.6V, not enough for what I need and mAh are around 8, is there as solution to this that I am missing?

thanks in advance

C

Can you confirm the voltage of your battery with a multimeter?

If the battery is operating fine, then there could be an issue with the LDO voltage regulator. Try probing the output pin of the LDO, it should be 3.3V.