Logomatic: empty files

Hello,

just got the Logomatic, got it running, but it only reates empty log files.

Settings are

MODE = 2

ASCII = Y

Frequency = 100

AD1.3 = Y

AD0.3 = N

AD0.2 = N

AD0.1 = N

AD1.2 = Y

AD0.4 = Y

AD1.7 = Y

AD1.6 = Y

Safety On = Y

want to do analogue measurments.

Cheers,

Steffen

edit: maybe I put it into a funny mode, reads values every minute or so.

It got

545 546 535 680 782

546 549 534 681 782

544 546 535 679 781

with open inputs

I will answer it myself somehow: as soon as one line is missing in the LOGCON.txt file it starts doing strange things. Had 6 inputs instead of 8 and readings every so often.