Hello everyone,
I am working on a project that uses several ADXL213 accelerometers to determine the stability of a vehicle in flight. I have the ADXL213’s set to analog output and want to use the logomatic to record the data during flight. I’ve tested the accelerometers with an ohmmeter to make sure they are work. I’ve wired them to the ADC on the logomatic but the logomatic just returns blank files every time. I have tried setting it to each mode and nothing works. I’ve tried the ‘hardware test mode’ as well but don’t really know if that should produce anything (it didn’t). The LED’s all light up like they should on start up but then just the USB light stays on (I’ve researched this and guess it’s not uncommon). I’m stumped, any help on this problem is greatly appreciated!