I am using the logomatic V2 combined with sleep cycles and big batteries for long term logging. My firmware is significantly different form the original but is based on it. I am 1) intermittently logging voltage into a text files when it is above a preset level and 2) continuously and logging the background voltage first into an array and then into a second file when the array fills. the first part seems to work very well and is reliable. The second part using file_open _append (thanks for that modification Iquaba ) seems to work for several cycles but after being left for 4 or 5 cycles, (and it may have something to do with logging a data file as in 1) the file becomes corrupted and will not open. Windows 7 can scan and fix the file but it ends up with a bunch of junk in the file, some of which looks like stuff destined for the data file (though all data files seem fine)
This behavior is a bit of a mystery to me and I would appreciate advice from someone with more SD card experience.
thanks,
Stefan