Logomatic Low freq?

Is there an expert could explain and let me know the exact settings I should apply to monitor at low frequency (in the range of 1 measurement/per hour) with the logomatic (data logger)?

If I understood correctly with T0MR0, which is a 32 bit variable, I can set to the maximum of 2^32 = 4294967296 → 4294967296 / 58982400 = 72 s.

Is there a way to get a slower frequency rate?

As I’m a novice, I would appreciate if you could let me know how the exact changes I have to do in the code of the main.c file?

Many thanks for your help.

Christoph

In case you want to operate the logomatic at down to 1 per min (0.01667 Hz), I’v modified the main.c file accordingly.

Set for instance in the logcon.txt file “Frequency = .01667”. Max 6 digits.