Logomatic V2 questions

How do you read the data collected by the data logger, with a spread sheet like Excel?

Is there a time stamp?

If I use two to have 16 inputs, can they be synchronized?

If I want to use one of the digital input, as a counter, do I have to do the programming myself?

That should be enough for now…

Thanks

Oups, more questions,

Can the Logomatic be made to store data directly to a computer without having to download the files manually?

When it says it can use a micro SD card of 1G, is that 1 Gyga “Bytes”?

If each readings use, lets say 2 bytes, I would have one half of a billion readings before the card is full?

Thanks again

For the first question you must just import; for the second question the answer is: not now. You have to work both HW and SW. For all other the answer is yes but for the third and fourth you must to work on sw.

Pier