Looking for connectors for Olimex header pins

Hi all,

I have a Olimex LPC-213X-B with 2138 on it. There are two rows of 2x16

header pins on both sides of the board. As a temporary solution I

attached a standard hdd cable with 2x20 pin female connectors from an

old computer. Then I cut out several cables from the 40way flat cable

and used them without a problem.

However these flat socket/cable combination is too bulky and I do not

need many pins. Therefore I want to replace both of them with 1/2/3 way

single row female sockets and connect them only to the pins I need.

But, I do not know the names and part numbers of such sockets, neither I

could locate them on the net. Please help.

Thanks

Cem Eryasar

I use these for that sort of application:

http://www.harwin.com/catalogue/search/ … artNumber=

You will need a suitable tool for crimping the terminals.

Leon

Or if you want the headers for prototyping board, try here:

http://www.futurlec.com/ConnHead.shtml

Regards,

Robert

I’ve had bad luck with futurlec… order was incomplete, late, and took weeks of back and forth to get some (not all) of the parts i ordered.