I have a question with LPC-E2294 board, when I received the board, both jumper 11 and jumper 13 are short in 1-2 that means memory width is 8 bits, the board works ok, but I look at schematic, i find the the flash is 16 bit memory interface, I think the jumper11 and 13 should set to 16 bits memory width, why is that ? Thanks
Can you please tell me the default settings (factory settings or settings for shipping) for jumper 11 and jumper 13 ? And also where the test program reside ? internal flash or 4 MB ex-flash ? Thank.