LPC2000 Flash ISP Utility, V2.2.3 - Anyone using it ?

I tried using the LPC2000 Flash ISP Utility. i got it to work on my LPC2148 but only up to 38400 baud. Has anyone else used this utility and got it working at a higher rate ?

I’ve been using FlashMagic sucessfully. It’s much better than LPC2000 Flash Utility. I believe that NXP has stopped work on their ISP Utility.

http://www.flashmagictool.com/

Mith

Table 291 in the user manual (p. 299) shows the baud rates that the 2148 is capable of with ISP with respect to your crystal frequency. I use version 2.2.3 and I also can only get up to 38400 with a 12 MHz crystal. There are only a few crystal frequencies that you can actually go higher than that with the LPC2000 flash utility. I might try out that FlashMagic tool if it’s quicker, though.

Table 291 in the user manual (p. 299) shows the baud rates that the 2148 is capable of with ISP with respect to your crystal frequency

Thanks, i caught that shortly after my post.

I changed my 12 mHz rock with a 14.7456mhz. and now i can get baud rates up to 230400 using FlashMagic.

Thanks Guys, i just wish we could use the onboard USB port to flash them too.