i have LPC2138 uber evaluation board, also i have downloaded LPC2000 flash utility from philips, but when i use it to download the HEX file into LPC2138 flash the below messages were generated:
I think you should first make sure that you don’t get the “cannot communicate with the test board” message anymore. Try lowering the baud rate (say 38400) and make sure you fill in the right crystal frequency in the Philips ISP tool.
i have LPC2138 uber evaluation board, also i have downloaded LPC2000 flash utility from philips, but when i use it to download the HEX file into LPC2138 flash the below messages were generated:
HEX file exceedes flash limitations.
cannot communicate with the test board
please help me
regards
What hex file are you trying to download? Was the application built properly for the LPC2138?
I have tried all the available baud rate on the flash utility software, no luck! It always come back to me with error message “Cannot communicate with test board!”.
I have tested the serial port, it work with other hardware, it works fine.
Open hyperterm and configure it for 19200 baud 8N1, then hold P0.14 low while resetting the board. Typing ? (question mark) into the hyperterm a few times should result in a “Synchronized” message from the boot loader.
Do you get any errors if you just load the hex file into the LPC2000 Flash Utility? You can do this by selecting “Buffer/Flash Buffer Operations” from the menu and then pressing the “Load Hex File” button.
Can you use the ISP tool to read out the device ID without errors? It sounds like from previous posts that this is probably failing as well.