Yes, with the Phillips Flash Utility, the BSL jumper was shorted and the DBG_E jumper was open. However, the utility does not have a selection for LPC2103, so I used LPC2104
Yes, with the Olimex JTAG TINY, the BSL jumper was open and the DBG_E jumper was shorted. Here is my openocd.cfg:
telnet_port 4444
gdb_port 3333
interface ft2232
ft2232_device_desc “Olimex OpenOCD JTAG TINY”
ft2232_layout “olimex-jtag”
ft2232_vid_pid 0x15ba 0x0004
jtag_speed 0
reset_config trst_and_srst srst_pulls_trst
jtag_device 4 0x1 0xf 0xe
jtag_nsrst_delay 2000
jtag_ntrst_delay 2000
daemon_startup reset
target arm7tdmi little run_and_halt 0 arm7tdmi
run_and_halt_time 0 30
working_area 0 0x40000000 0x1000 nobackup
flash bank lpc2000 0x0 0x20000 0 0 0 lpc2000_v1 14745 calc_checksum
This is the contents of /proc/bus/usb/devices:
T: Bus=01 Lev=00 Prnt=00 Port=00 Cnt=00 Dev#= 1 Spd=12 MxCh= 4
B: Alloc= 0/900 us ( 0%), #Int= 0, #Iso= 0
D: Ver= 1.10 Cls=09(hub ) Sub=00 Prot=00 MxPS=64 #Cfgs= 1
P: Vendor=0000 ProdID=0000 Rev= 2.06
S: Manufacturer=Linux 2.6.23.1-21.fc7PAE ohci_hcd
S: Product=OHCI Host Controller
S: SerialNumber=0000:02:00.0
C:* #Ifs= 1 Cfg#= 1 Atr=e0 MxPwr= 0mA
I:* If#= 0 Alt= 0 #EPs= 1 Cls=09(hub ) Sub=00 Prot=00 Driver=hub
E: Ad=81(I) Atr=03(Int.) MxPS= 2 Ivl=255ms
T: Bus=01 Lev=01 Prnt=01 Port=01 Cnt=01 Dev#= 3 Spd=12 MxCh= 0
D: Ver= 2.00 Cls=00(>ifc ) Sub=00 Prot=00 MxPS= 8 #Cfgs= 1
P: Vendor=15ba ProdID=0004 Rev= 5.00
S: Manufacturer=Olimex
S: Product=Olimex OpenOCD JTAG TINY
S: SerialNumber=FTPX9R4V
C:* #Ifs= 2 Cfg#= 1 Atr=80 MxPwr=100mA
I:* If#= 0 Alt= 0 #EPs= 2 Cls=ff(vend.) Sub=ff Prot=ff Driver=(none)
E: Ad=81(I) Atr=02(Bulk) MxPS= 64 Ivl=0ms
E: Ad=02(O) Atr=02(Bulk) MxPS= 64 Ivl=0ms
I:* If#= 1 Alt= 0 #EPs= 2 Cls=ff(vend.) Sub=ff Prot=ff Driver=(none)
E: Ad=83(I) Atr=02(Bulk) MxPS= 64 Ivl=0ms
E: Ad=04(O) Atr=02(Bulk) MxPS= 64 Ivl=0ms
Here is the output when starting openocd:
root@maps mike]# openocd
Info: openocd.c:93 main(): Open On-Chip Debugger (2007-09-05 09:00 CEST)
Error: jtag.c:1253 jtag_examine_chain(): JTAG communication failure, check connection, JTAG interface, target power etc.
Error: jtag.c:1440 jtag_init(): trying to validate configured JTAG chain anyway…
Error: jtag.c:1346 jtag_validate_chain(): Error validating JTAG scan chain, IR mismatch, scan returned 0x3f
Error: jtag.c:1346 jtag_validate_chain(): Error validating JTAG scan chain, IR mismatch, scan returned 0x3f
Error: jtag.c:1346 jtag_validate_chain(): Error validating JTAG scan chain, IR mismatch, scan returned 0x3f
Error: jtag.c:1346 jtag_validate_chain(): Error validating JTAG scan chain, IR mismatch, scan returned 0x3f
Error: jtag.c:1346 jtag_validate_chain(): Error validating JTAG scan chain, IR mismatch, scan returned 0x3f
Error: jtag.c:1346 jtag_validate_chain(): Error validating JTAG scan chain, IR mismatch, scan returned 0x3f
Error: jtag.c:1448 jtag_init(): Could not validate JTAG chain, exit
[root@maps mike]#
Thanks