I am trying to get openocd 0.3.0 (latest from GIT) to work with my LPC2138 board.
I am running under WinXP/cygwin, and have built openocd this way.
I am running the following config for openocd:
file lpc2138.cfg:
if { [info exists CHIPNAME] } {
   set _CHIPNAME $CHIPNAME
} else {
   set _CHIPNAME lpc2138
}
if { [info exists ENDIAN] } {
   set _ENDIAN $ENDIAN
} else {
   set _ENDIAN little
}
if { [info exists CPUTAPID ] } {
   set _CPUTAPID $CPUTAPID
} else {
   set _CPUTAPID 0x4f1f0f0f
}
jtag_nsrst_delay 200
jtag_ntrst_delay 200
# NOTE!!! LPCs need reset pulled while RTCK is low. 0 to activate
# JTAG, power-on reset is not enough, i.e. you need to perform a
# reset before being able to talk to the LPC2148, attach is not possible.
reset_config trst_and_srst srst_pulls_trst
jtag newtap $_CHIPNAME cpu -irlen 4 -ircapture 0x1 -irmask 0xf -expected-id $_CPUTAPID
set _TARGETNAME $_CHIPNAME.cpu
target create $_TARGETNAME arm7tdmi -endian $_ENDIAN -chain-position $_TARGETNAME -variant arm7tdmi-s_r4
$_TARGETNAME configure -work-area-virt 0 -work-area-phys 0x40000000 -work-area-size 0x8000 -work-area-backup 0
$_TARGETNAME configure -event reset-init {
	# Force target into ARM state.
	soft_reset_halt
	# Do not remap 0x0000-0x0020 to anything but the flash (i.e. select
	# "User Flash Mode" where interrupt vectors are _not_ remapped,
	# and reside in flash instead).
	#
	# See section 7.1 on page 32 ("Memory Mapping control register") in
	# "UM10120".
	#
	mwb 0xE01FC040 0x01
#	jtag_khz 1500
}
# flash bank lpc2000 <base> <size> 0 0 <target#> <variant> <clock> [calc_checksum]
flash bank lpc2000 0x0 0x7d000 0 0 0 lpc2000_v2 14765 calc_checksum
testconfig.cfg:
source [find tcl/target/lpc2138.cfg]
source [find tcl/interface/olimex-jtag-tiny.cfg]
# tell gdb our flash memory map
# and enable flash programming
gdb_memory_map enable
gdb_flash_program enable
#daemon configuration
telnet_port 4444
gdb_port 3333
jtag_speed 3
init
reset init
I am running openocd with the command “openocd.exe -d 3 -f testconfig.cfg”, and I am then running this set of commands using gdb from within eclipse:
target remote localhost:3333
monitor reset init
monitor sleep 500
#monitor poll
monitor soft_reset_halt
monitor mww 0xE01FC040 0x0002
monitor mdw 0xE01FC040
needed for gdb 6.8 and higher
set mem inaccessible-by-default off
load
break main
continue
I can connect to the lpc2138 and all, but I cant seem to get the target halted as all goes wrong as soon as I perform the first monitor-command.
The flash-based program in the LPC blinks a LED, and this stops after executing “monitor soft_reset_halt”, while OCD doesn’t seem to believe the target to be halted.
Anyone see anything wrong with my approach?