Hello,
i just receive a LPC2478-STK evaluation board from OLIMEX and i would like to flash U-BOOT on it with Flash Magic (for testing flashing procedure) but i can’t because i always have “Failed to autobaud - step 1”. I have configure ,
Step 1 as :
Device : LPC2478
COM Port : COM 1 (real com port from PC, not FTDI)
Baud rate : 9600
Interface : None (ISP)
Oscillator (MHz) : 12
Step 2 as :
tick “Erase all Flash+Code Rd Prot”
Step 3 Hex File from correct location
Step 4 : None tick
I can’t go to flash magic forum because of my enterprise internet restriction (it sucks !, sorry).
Then can anyone help me to find correct procedure ?
Thanks a lot
PS : In normal operation ,the board boot correctly ,i see penguin on LCD and text on PC COM1 terminal , i can entering into UBOOT menu or let uclinux boot on USB mass storage