LTC3588-1 Pin locations

I bought your Ltc3588 module to use in our senior design project. Our project name is ‘Energy Harvesting by Piezoelectric at Smart Textile’. Our piezo source is LDT0-028K. The pins shown in the datasheet do not match the pins of the module in my hand, so I cannot apply the circuits you have installed. Is the circuit you have installed under the title ‘Typical Application’ integrated circuit in the module?

The pin connections are labeled on the bottom silkscreen and match those of the schematic.

The schematic for the module can be found at https://www.sparkfun.com/datasheets/Bre … er-v12.pdf It looks the same as the one in the data sheet except the output cap is 10uF on the board and 47uF on the data sheet

/mike