This issue is usually related to either a power or connection issue. What are you using to power the RedBoard+M6E Nano? To identify whether or not there is a connection issue, please take a few photos of the top and bottom of your Simultaneous RFID Reader and attach them to your response? Also, make sure the HW UART/SW UART switch is in the SW position. Finally, what example code from the library are you using?
I too have this issue. I have connected the sparkfun simultaneous rfid tag reader to an FTDI TTL-232R 5V ttl to usb serial converter. The switch is set to SW-UART ( though I get the same error when set to HW-UART). When I run the URA I get the following error:
“Unable to connect to USB Serial Port (COM20). Please Check if the device is properly connected or Device might be in use.”
I have ensured that 5V is being supplied to the board, and that the connections to the FTDI Chip are correctly made. Looking at the serial port connections on the SRTR to the left the connections from my cable are as follows:
Open your com port using a terminal program (PUTTY, TeraTerm, etc).
Type some characters and ensure that they are showing up on the screen (one per keypress if you have local echo disabled, twice if enabled in the terminal program)
If this doesn’t work, the issue is on with the PC, FTDI driver, or FTDI cable.
The correct drivers are installed for the FTDI chip. I checked this in bot the device manager and by successfully performing the check that Mike suggested.
The SRTR is NOT connected to an Arduino and you are correct nothing is connected to enable . The power light is on and I have since tried using a bench supply in place of USB power, but I get the same problem.
I have tried switching yellow and orange, still the same issue.
When I initially start up the URA I’m presented with the Connection wizard which provides the Error “Unable to connect to USB Serial Port (COM20). Please Check if the device is properly connected or Device might be in use.” when I click next.
If I skip the connection wizard and attempt to connect as per the sparkfun guide the error message changes to “Error connecting to reader: Timeout Exception”
As an Update to this I have now tried an older release of the URA and still no joy. I have also tried a different USB to serial cable which gave the same problems, as well as trying the same tests on a different USB port, and then a different Host PC all to no luck. I am completely stumped as to what to do next. If anyone has had this problem before advice is greatly received.
It may be a hardware issue. Can you please take a few photos of the top and bottom of the Simultaneous RFID Reader and attach them to your reply? Especially any soldering you have done.
During connect that URA tries to connect to M6E with different speeds. If it fails after trying 8 or 9 different speeds you will get this error message. I expect if you make a transport log with the URA we will see the different attempts. Maybe try it and share that transport log.
I assume you are using the VCP driver and not the D2XX. did you load the latest from the version from the website ?
I only had one situation where I could NOT connect with the M6E, which was with an ESP32. As that uses 3V3, I needed a level converter. The on-board level convertor on the M6E Nano (TXB0104) did not work well with the external level convertor and I needed to make a resistor bridge to make it work.
One other thought that COULD be an issue (but unlikely as it works on the Redboard) is the M6E firmware. I would not try that change with the URA at this stage however.
I have since tried using the spark fun red board and the arduino examples. Good news, these work fine. For now I will be progressing my testing using these examples rather than the URA.
What I can say is, the Nano board works, hopefully at some point I will try get round to answering why the URA software doesn’t and the FTDI lead doesn’t.