Hello all!
I’ve been trying to connect the the M7E in my Flutter Android app, but I’ve been having some trouble. I’ve got an Android tablet running a Flutter app and in that Flutter app I detect when the M7E is connected via USB to the tablet. I then request USB permissions and connect to the M7E. The problems start when I try to connect to the M7E. I’m constantly getting the following errors when I try to execute the reader.connect() command:
E/AndroidUSBTransport( 8573): java.lang.NullPointerException: Attempt to invoke virtual method 'java.lang.Class java.lang.Object.getClass()' on a null object reference
E/AndroidUSBTransport( 8573): at com.thingmagic.AndroidUsbReflection.isOpen(AndroidUsbReflection.java:177)
E/AndroidUSBTransport( 8573): at com.thingmagic.AndroidUSBTransport.open(AndroidUSBTransport.java:98)
E/AndroidUSBTransport( 8573): at com.thingmagic.SerialReader.openSerialPort(SerialReader.java:16400)
E/AndroidUSBTransport( 8573): at com.thingmagic.SerialReader.openPort(SerialReader.java:16411)
E/AndroidUSBTransport( 8573): at com.thingmagic.SerialReader.connect(SerialReader.java:11077)
E/AndroidUSBTransport( 8573): at com.example.rfid_test_flutter_v3_29.MainActivity$setupRFID$1.invokeSuspend(oldMainActivity.kt:157)
E/AndroidUSBTransport( 8573): at kotlin.coroutines.jvm.internal.BaseContinuationImpl.resumeWith(ContinuationImpl.kt:33)
E/AndroidUSBTransport( 8573): at kotlinx.coroutines.DispatchedTask.run(DispatchedTask.kt:106)
E/AndroidUSBTransport( 8573): at kotlinx.coroutines.internal.LimitedDispatcher$Worker.run(LimitedDispatcher.kt:115)
E/AndroidUSBTransport( 8573): at kotlinx.coroutines.scheduling.TaskImpl.run(Tasks.kt:100)
E/AndroidUSBTransport( 8573): at kotlinx.coroutines.scheduling.CoroutineScheduler.runSafely(CoroutineScheduler.kt:584)
E/AndroidUSBTransport( 8573): at kotlinx.coroutines.scheduling.CoroutineScheduler$Worker.executeTask(CoroutineScheduler.kt:793)
E/AndroidUSBTransport( 8573): at kotlinx.coroutines.scheduling.CoroutineScheduler$Worker.runWorker(CoroutineScheduler.kt:697)
E/AndroidUSBTransport( 8573): at kotlinx.coroutines.scheduling.CoroutineScheduler$Worker.run(CoroutineScheduler.kt:684)
E/SetupRFID( 8573): Failed to setup reader
E/SetupRFID( 8573): com.thingmagic.ReaderException: Couldn't open device
E/SetupRFID( 8573): at com.thingmagic.AndroidUSBTransport.open(AndroidUSBTransport.java:110)
E/SetupRFID( 8573): at com.thingmagic.SerialReader.openSerialPort(SerialReader.java:16400)
E/SetupRFID( 8573): at com.thingmagic.SerialReader.openPort(SerialReader.java:16411)
E/SetupRFID( 8573): at com.thingmagic.SerialReader.connect(SerialReader.java:11077)
E/SetupRFID( 8573): at com.example.rfid_test_flutter_v3_29.MainActivity$setupRFID$1.invokeSuspend(oldMainActivity.kt:157)
E/SetupRFID( 8573): at kotlin.coroutines.jvm.internal.BaseContinuationImpl.resumeWith(ContinuationImpl.kt:33)
E/SetupRFID( 8573): at kotlinx.coroutines.DispatchedTask.run(DispatchedTask.kt:106)
E/SetupRFID( 8573): at kotlinx.coroutines.internal.LimitedDispatcher$Worker.run(LimitedDispatcher.kt:115)
E/SetupRFID( 8573): at kotlinx.coroutines.scheduling.TaskImpl.run(Tasks.kt:100)
E/SetupRFID( 8573): at kotlinx.coroutines.scheduling.CoroutineScheduler.runSafely(CoroutineScheduler.kt:584)
E/SetupRFID( 8573): at kotlinx.coroutines.scheduling.CoroutineScheduler$Worker.executeTask(CoroutineScheduler.kt:793)
E/SetupRFID( 8573): at kotlinx.coroutines.scheduling.CoroutineScheduler$Worker.runWorker(CoroutineScheduler.kt:697)
E/SetupRFID( 8573): at kotlinx.coroutines.scheduling.CoroutineScheduler$Worker.run(CoroutineScheduler.kt:684)
Here is the Kotlin code that I’m using to connect to the reader:
private fun setupRFID(result: MethodChannel.Result) {
CoroutineScope(Dispatchers.IO).launch {
try {
if (currentDevice == null || !usbManager.hasPermission(currentDevice)) {
result.error("USB_ERROR", "No USB permission or device", null)
return@launch
}
Log.d("USB", "Using device: ${currentDevice?.deviceName}, VID=${currentDevice?.vendorId}, PID=${currentDevice?.productId}")
reader = SerialReader.create("tmr:///dev/ttyUSB0")
// SerialReader.setSerialTransport(AndroidUSBTransport(currentDevice, usbManager))
reader?.connect()
reader?.paramSet("/reader/region/id", Reader.Region.NA)
Log.d("SetupRFID", "Reader setup complete - $reader")
result.success("Reader setup complete")
} catch (e: Exception) {
Log.e("SetupRFID", "Failed to setup reader", e)
result.error("SETUP_ERROR", e.message, e)
}
}
}
I have downloaded the [ ThingMagic® Mercury API BILBO 1.37.3.29] from the Jadak website and I went into the Java directory, found the sample Android project and copied the files in the sample project’s libs folder into my project’s libs folder. So I have 4 files in my Android libs folder:
- d2xx.jar
- jmdns-3.4.1.jar
- ltkjava-1.0.0.6.jar
- mercuryapi.jar
Does anybody have an idea of what I might be doing wrong? Am I creating the SerialReader with the wrong uri? Is it even possible to control the M7E from an Android app? I’ve been trying to follow the Mercury API’s programmer guide but I haven’t seen anything in there about this.
I look forward to hearing from everyone!