Could someone please tell me what is the maximum current that can be drawn from the VOUT pin of the LPC1768 based Mbed board? I tried looking for this information in the datasheet, but couldn’t find it. Maybe I’m not looking at the right place.
I’m trying to connect the sparkfun Nokia LCD board, and the JPEG camera with the mbed, and I’m wondering if I can draw 484mA (324mA for the backlight, 100mA for the LCD and 60mA for the JPEG camera) from the VOUT pin directly. That would save me the trouble of using another 3.3v supply.
Could someone also point me to the electrical specifications of the mbed? I am somehow unable to find detailed specifications anywhere, which is kind of surprising for an NXP product.
@rmteo1: Thanks. I had already seen that link, it doesn’t exactly specify how much current load the VOUT pin can bear.
Anyhow, for anybody interested in the future, I went through the schematics of the mbed, it has two LD1117S33 regulators, one for powering the internal 3.3v used by the board and one for VOUT. The regulator has a maximum load of 800mA.