Microview driver ?

Hello all,

I would like to be able to use my Microview with BASCOM but that requires using the arduino drivers.

When I try to update the driver, using the uno for example, bad things happen to my XP machine.

It resets my XP machine every time I plug in the Microview with the Programmer.

Does anyone know which arduino driver can be used instead of being setup as a Virtual Com Port ?

Regards Larry

Hi Lander72,

If you are using the MicroView’s factory USB programmer, then you need the FTDI driver

http://www.ftdichip.com/Drivers/VCP.htm

Please refer to “Install Driver” section

http://learn.microview.io/intro/getting-started.html

Hope this helps.

Cheers

JP

Thanks for the reply. I was hopeful that there was a possibility to use the Uno driver;

May I know if you are facing any constraint that is preventing you from using a virtual com port?

As far as I know, most Arduinos are using virtual com port including uno. Uno is using ATmega8 or 16 to act as a virtual com port.