I would like to monitor the 12V battery supply to my Arduino. The goal is to provide an indication, in the form of a blinking LED, when the supply voltage falls below 10V. I propose to do this by making Vin = to the supply voltage and dividing this reference to 5V or less using a voltage divider. I could then measure the battery voltage by using the ADC on one of the analog pins. By monitoring the ADC voltage periodically, I could turn on the blinking LED when the supply voltage fell to or below 10V. Is this a workable solution? Other suggestions?
Any enlightenment will be appreciated.
Vic