Hello and thank you for helping me,
I have recently embarked on a project which requires amperage above 3A and possibly up to 15A or so. I understand these N-channel MOSFETs are well capable of handling this current but I can not understand how you would set this up. Solder-less breadboards are not safe for that current and solder-able breadboards apparently should not take currents this high even if you leave a solder trace because their resistance is quite high causing more heat. The terminals off the MOSFET are so tiny and close together, they are nearly impossible to solder directly to the wires so I do not understand how their full potential can be maximized. I use MOSFETs in general because nearly all from cheap to those from Texas Instruments can handle absurd amounts of power if properly heat-sinked. May someone please help me find an alternative to moving forward.
Thank you,
Adam