Hi,
I am using the MSP430-JTAG-ISO to connect to an electric meter running at 120 VAC. My target board is now floating at 120 VAC. I have tried two MSP430-JTAG-ISO units. The first unit would not work at all. The second unit seemed to work for a day but now I can no longer connect. I receive either “Cannot set VCC” or “VCC too high: 3.6V”.
I have tried multiple setups:
VAC to Isolation XFMR to electric meter
VAC to Isolation XFRM to Computer to MSP430-JTAG-ISO
The electric meter has a 15 VDC unregulated supply that I am regulating to 3.3 VDC that supplies my target board. I have also tried disconnecting the 15 VDC and supplying the 3.6 VDC via a battery. No luck.
Has anyone had any luck with the MSP430-JTAG-ISO in a situation? Any ideas on what could be going on?
Thanks
Duane.