The title says it all. I do all my development/testing on linux.
I purchased the TI parallel port adaptor a long time ago and do my development with this. But these devices are slow. I’ve since purchased two JTAG-ISO devices because they can read and write the program standalone in seconds vs minutes for the TI version. This is great for releasing to production.
I would love to use only the JTAG-ISO device during development, but the libHIL.so from the mspgcc group only supports parallel port.
Any chance of getting support for usb? I might be able to offer some help if it is just a development time problem. I’m very familiar with libusb under linux, and of course the gdbproxy code is open source. All that is needed is a libHIL which talks usb I think.
Actually, the msp430 gdbproxy is not completely open source. The key low-level code that talks to the chip is proprietary to TI. This will become apparent to you if you try to figure out what the gdbproxy source code is doing.
I remember reading somewhere that someone was working on a linux usb solution using closed code from TI but I never heard what became of that effort.
If you request the details from TI and you sign a non-disclosure agreement they’ll send you a nice package with a lot of info. Unfortunately, this documents the msp430.dll API, which is obviously not portable to linux (unless WINE might work?). Maybe if you explain why you need the info they’ll let you have the REAL chip-level info.
I have no idea why TI is so protective of this info. It seems like all the chip makers have their own on-chip debugging module, but only Freescale publicly documents the low-level details.
Please let us know if you get the info and are able to make a module others can use. It’s understandable that you can’t tell anyone the trade secrets, but maybe it can be distributed in a binary format.
The TI version of the MSP430UIF (i.e. with USB interface) interface code is available from TI. I have a copy of it and have put some of it (the main functions) into open source form and distributed it (without any warrenty). We use it for our production testing.
The OLIMEX devices, however, use a different interface. Both the TI and the OLIMEX interface are based on serial ASYNC communications and both have
on-board microprocessors, but otherwise the designs are different. I have tried to get the OLIMEX interface description but it has not been forthcoming.
If you want a USB interface (and who doesn’t, it is so much faster), then you are stuck buying the TI MSP430UIF for $99.
I know it is a little bit late since 2006 but I’ve been working on a free library to handle the OLIMEX MSP430 JTAG ISO under linux. It currently works with my own under Linux, Windows and MacOSX.
The project is named FMDLL which stands for Free MSP430 Debugger Link Library and is available @ :
The project is still under development but works fine to erase, load, and debug code.
I hope this will help you.
PS: Usage with msp430-gdbproxy is documented on the web site. I’m working on a free implementation of the msp430 module of gdbproxy which will be open-source.