Hello,
does someone knows how to receive data from 2 differents funnel io(both using firmata) into max (maxuino or serial) using only one xbee usb explorer receiver?
I am actually on snow leopard 10.6.7
I have 2 funnel fio, both use a xbee module serie 1 and firmata as end devices.
then i got a xbee plugged into a usb xbee explorer as a coordinator/receiver.
end of the chain is max/msp with maxuino.
for the xbee config
3 modules got the Pan ID 1234
funnel xbee 1 got ID 0001
funnel xbee 2 got ID 0002
The coordinator Pan ID is 1234 there is no My ID for coordinator
and the funnel are 0 and 1 on pan ID 1234.
if i run the boards separately its working perfect.
when i got the both running, the first one connected is working with maxuino, the second one send me that message on the max windows
[arduino]_WARNING_INCOMPATIBLE_FIRMWARE_VERSION: 2
Arduino/Firmata_version: 2 2
Does Someone can help me to deal with that??
thank you
Freeka