Multiple schematics sheets in free Eagle

I can make the fat lady spin on her toe like a ballerina.

(Generating gerber files is the fat lady singing).

It’s actually 1 big sheet (2 A size frames in length).

The longer sheet prints across 2 sheets.

If I put 2 more frames I can go to 4 A size sheets.

Eagle free version only supports 1 sheet but it can be any size.

The frame is a library component so I put 2.

I check the print preview to position the other frame and tweak the scale.

I found that a gap of .5 between frames and a scale of .94 is perfect.

Both title boxes say page 1 of 1, but the title box is just a part too so just make another.

Now I don’t have to print larger sheets at Office Max.

Who says free Eagle only supports 1 schematic sheet, I beg to differ.

In your face CadSoft!!

KD6KCA

Just curious what version of eagle are you using?